RTC_Init_TypeDef Struct ReferenceEMLIB > RTC
RTC initialization structure.
Definition at line 71
of file em_rtc.h
.
#include <
em_rtc.h
>
Data Fields | |
bool | comp0Top |
bool | debugRun |
bool | enable |
Field Documentation
bool RTC_Init_TypeDef::comp0Top |
Use compare register 0 as max count value.
Definition at line 74
of file em_rtc.h
.
Referenced by RTC_Init(), and UDELAY_Calibrate().
bool RTC_Init_TypeDef::debugRun |
Counter shall keep running during debug halt.
Definition at line 73
of file em_rtc.h
.
Referenced by RTC_Init().
bool RTC_Init_TypeDef::enable |
Start counting when initialization is completed.
Definition at line 72
of file em_rtc.h
.
Referenced by RTC_Init().
The documentation for this struct was generated from the following file:
- C:/repos/super_h1/platform/emlib/inc/
em_rtc.h