LETIMEREMLIB
Detailed Description
Low Energy Timer (LETIMER) Peripheral API.
This module contains functions to control the LETIMER peripheral of Silicon Labs 32-bit MCUs and SoCs. The LETIMER is a down-counter that can keep track of time and output configurable waveforms.
         Data Structures | 
       |
| struct | LETIMER_Init_TypeDef | 
         Macros | 
       |
| #define | LETIMER_INIT_DEFAULT | 
         Enumerations | 
       |
| enum | 
         
          LETIMER_RepeatMode_TypeDef
         
         {
          letimerRepeatFree = _LETIMER_CTRL_REPMODE_FREE, letimerRepeatOneshot = _LETIMER_CTRL_REPMODE_ONESHOT, letimerRepeatBuffered = _LETIMER_CTRL_REPMODE_BUFFERED, letimerRepeatDouble = _LETIMER_CTRL_REPMODE_DOUBLE }  | 
       
| enum | 
         
          LETIMER_UFOA_TypeDef
         
         {
          letimerUFOANone = _LETIMER_CTRL_UFOA0_NONE, letimerUFOAToggle = _LETIMER_CTRL_UFOA0_TOGGLE, letimerUFOAPulse = _LETIMER_CTRL_UFOA0_PULSE, letimerUFOAPwm = _LETIMER_CTRL_UFOA0_PWM }  | 
       
         Functions | 
       |
| uint32_t | LETIMER_CompareGet ( LETIMER_TypeDef *letimer, unsigned int comp) | 
| 
         Get the LETIMER compare register value.
          | 
       |
| void | LETIMER_CompareSet ( LETIMER_TypeDef *letimer, unsigned int comp, uint32_t value) | 
| 
         Set the LETIMER compare register value.
          | 
       |
| __STATIC_INLINE uint32_t | LETIMER_CounterGet ( LETIMER_TypeDef *letimer) | 
| 
         Get LETIMER counter value.
          | 
       |
| void | LETIMER_Enable ( LETIMER_TypeDef *letimer, bool enable) | 
| 
         Start/stop LETIMER.
          | 
       |
| void | LETIMER_FreezeEnable ( LETIMER_TypeDef *letimer, bool enable) | 
| 
         LETIMER register synchronization freeze control.
          | 
       |
| void | LETIMER_Init ( LETIMER_TypeDef *letimer, const LETIMER_Init_TypeDef *init) | 
| 
         Initialize LETIMER.
          | 
       |
| __STATIC_INLINE void | LETIMER_IntClear ( LETIMER_TypeDef *letimer, uint32_t flags) | 
| 
         Clear one or more pending LETIMER interrupts.
          | 
       |
| __STATIC_INLINE void | LETIMER_IntDisable ( LETIMER_TypeDef *letimer, uint32_t flags) | 
| 
         Disable one or more LETIMER interrupts.
          | 
       |
| __STATIC_INLINE void | LETIMER_IntEnable ( LETIMER_TypeDef *letimer, uint32_t flags) | 
| 
         Enable one or more LETIMER interrupts.
          | 
       |
| __STATIC_INLINE uint32_t | LETIMER_IntGet ( LETIMER_TypeDef *letimer) | 
| 
         Get pending LETIMER interrupt flags.
          | 
       |
| __STATIC_INLINE uint32_t | LETIMER_IntGetEnabled ( LETIMER_TypeDef *letimer) | 
| 
         Get enabled and pending LETIMER interrupt flags.
          | 
       |
| __STATIC_INLINE void | LETIMER_IntSet ( LETIMER_TypeDef *letimer, uint32_t flags) | 
| 
         Set one or more pending LETIMER interrupts from SW.
          | 
       |
| uint32_t | LETIMER_RepeatGet ( LETIMER_TypeDef *letimer, unsigned int rep) | 
| 
         Get the LETIMER repeat register value.
          | 
       |
| void | LETIMER_RepeatSet ( LETIMER_TypeDef *letimer, unsigned int rep, uint32_t value) | 
| 
         Set the LETIMER repeat counter register value.
          | 
       |
| void | LETIMER_Reset ( LETIMER_TypeDef *letimer) | 
| 
         Reset LETIMER to the same state that it was in after a hardware reset.
          | 
       |
| void | LETIMER_SyncWait ( LETIMER_TypeDef *letimer) | 
| 
         Wait for the LETIMER to complete all synchronization of register changes and commands.
          | 
       |
| __STATIC_INLINE uint32_t | LETIMER_TopGet ( LETIMER_TypeDef *letimer) | 
| 
         Get the current LETIMER top value.
          | 
       |
| void | LETIMER_TopSet ( LETIMER_TypeDef *letimer, uint32_t value) | 
| 
         Set the LETIMER top value.
          | 
       |
Macro Definition Documentation
| #define LETIMER_INIT_DEFAULT | 
Default configuration for LETIMER initialization structure.
        Definition at line
        
         111
        
        of file
        
         em_letimer.h
        
        .
       
Referenced by MIC_init() .
Enumeration Type Documentation
Repeat mode.
        Definition at line
        
         58
        
        of file
        
         em_letimer.h
        
        .
       
| enum LETIMER_UFOA_TypeDef | 
Underflow action on output.
        Definition at line
        
         76
        
        of file
        
         em_letimer.h
        
        .
       
Function Documentation
| uint32_t LETIMER_CompareGet | ( | LETIMER_TypeDef * | 
           
            letimer,
           
           | 
         
| unsigned int | 
           
            comp
           
           | 
         ||
| ) | 
Get the LETIMER compare register value.
- Parameters
 - 
         
[in] letimerA pointer to the LETIMER peripheral register block. [in] compA compare register to get, either 0 or 1.  
- Returns
 - A compare register value, 0 if invalid register selected.
 
        Definition at line
        
         134
        
        of file
        
         em_letimer.c
        
        .
       
References LETIMER_TypeDef::COMP0 , and LETIMER_TypeDef::COMP1 .
| void LETIMER_CompareSet | ( | LETIMER_TypeDef * | 
           
            letimer,
           
           | 
         
| unsigned int | 
           
            comp,
           
           | 
         ||
| uint32_t | 
           
            value
           
           | 
         ||
| ) | 
Set the LETIMER compare register value.
- Note
 - The setting of a compare register requires synchronization into the low frequency domain. If the same register is modified before a previous update has completed, this function will stall until the previous synchronization has completed. This only applies to the Gecko Family. See comments in the LETIMER_Sync() internal function call.
 
- Parameters
 - 
         
[in] letimerA pointer to the LETIMER peripheral register block. [in] compA compare register to set, either 0 or 1. [in] valueAn initialization value (<= 0x0000ffff).  
        Definition at line
        
         179
        
        of file
        
         em_letimer.c
        
        .
       
References _LETIMER_COMP0_COMP0_MASK , _LETIMER_COMP0_COMP0_SHIFT , LETIMER_TypeDef::COMP0 , LETIMER_TypeDef::COMP1 , LETIMER_SYNCBUSY_COMP0 , and LETIMER_SYNCBUSY_COMP1 .
Referenced by LETIMER_TopSet() , and MIC_init() .
| __STATIC_INLINE uint32_t LETIMER_CounterGet | ( | LETIMER_TypeDef * | 
           
            letimer
           
           | 
          ) | 
Get LETIMER counter value.
- Parameters
 - 
         
[in] letimerPointer to the LETIMER peripheral register block.  
- Returns
 - Current LETIMER counter value.
 
        Definition at line
        
         161
        
        of file
        
         em_letimer.h
        
        .
       
References LETIMER_TypeDef::CNT .
| void LETIMER_Enable | ( | LETIMER_TypeDef * | 
           
            letimer,
           
           | 
         
| bool | 
           
            enable
           
           | 
         ||
| ) | 
Start/stop LETIMER.
- Note
 - The enabling/disabling of the LETIMER modifies the LETIMER CMD register which requires synchronization into the low-frequency domain. If this register is modified before a previous update to the same register has completed, this function will stall until the previous synchronization has completed. This only applies to the Gecko Family. See comments in the LETIMER_Sync() internal function call.
 
- Parameters
 - 
         
[in] letimerA pointer to the LETIMER peripheral register block. [in] enableTrue to enable counting, false to disable.  
        Definition at line
        
         232
        
        of file
        
         em_letimer.c
        
        .
       
References LETIMER_TypeDef::CMD , LETIMER_CMD_START , LETIMER_CMD_STOP , LETIMER_SYNCBUSY_CMD , and LETIMER_TypeDef::SYNCBUSY .
| void LETIMER_FreezeEnable | ( | LETIMER_TypeDef * | 
           
            letimer,
           
           | 
         
| bool | 
           
            enable
           
           | 
         ||
| ) | 
LETIMER register synchronization freeze control.
Some LETIMER registers require synchronization into the low-frequency (LF) domain. The freeze feature allows for several such registers to be modified before passing them to the LF domain simultaneously (which takes place when the freeze mode is disabled).
- Note
 - When enabling freeze mode, this function will wait for all current ongoing LETIMER synchronization to the LF domain to complete (Normally synchronization will not be in progress.) However, for this reason, when using freeze mode, modifications of registers requiring the LF synchronization should be done within one freeze enable/disable block to avoid unecessary stalling.
 
- Parameters
 - 
         
[in] letimerA pointer to the LETIMER peripheral register block. [in] enable- True - enable freeze, modified registers are not propagated to the LF domain
 - False - disables freeze, modified registers are propagated to the LF domain
 
 
        Definition at line
        
         280
        
        of file
        
         em_letimer.c
        
        .
       
References LETIMER_TypeDef::FREEZE , LETIMER_FREEZE_REGFREEZE , and LETIMER_TypeDef::SYNCBUSY .
Referenced by LETIMER_Reset() .
| void LETIMER_Init | ( | LETIMER_TypeDef * | 
           
            letimer,
           
           | 
         
| const LETIMER_Init_TypeDef * | 
           
            init
           
           | 
         ||
| ) | 
Initialize LETIMER.
Note that the compare/repeat values must be set separately with LETIMER_CompareSet() and LETIMER_RepeatSet() . That should probably be done prior using this function if configuring the LETIMER to start when initialization is complete.
- Note
 - The initialization of the LETIMER modifies the LETIMER CTRL/CMD registers which require synchronization into the low-frequency domain. If any of those registers are modified before a previous update to the same register has completed, this function will stall until the previous synchronization has completed. This only applies to the Gecko Family. See comments in the LETIMER_Sync() internal function call.
 
- Parameters
 - 
         
[in] letimerA pointer to the LETIMER peripheral register block. [in] initA pointer to the LETIMER initialization structure.  
        Definition at line
        
         326
        
        of file
        
         em_letimer.c
        
        .
       
References _LETIMER_CTRL_REPMODE_SHIFT , _LETIMER_CTRL_UFOA0_SHIFT , _LETIMER_CTRL_UFOA1_SHIFT , LETIMER_Init_TypeDef::bufTop , LETIMER_TypeDef::CMD , LETIMER_TypeDef::COMP0 , LETIMER_Init_TypeDef::comp0Top , LETIMER_TypeDef::CTRL , LETIMER_Init_TypeDef::debugRun , LETIMER_Init_TypeDef::enable , LETIMER_CMD_START , LETIMER_CMD_STOP , LETIMER_CTRL_BUFTOP , LETIMER_CTRL_COMP0TOP , LETIMER_CTRL_DEBUGRUN , LETIMER_CTRL_OPOL0 , LETIMER_CTRL_OPOL1 , LETIMER_CTRL_RTCC0TEN , LETIMER_CTRL_RTCC1TEN , LETIMER_STATUS_RUNNING , LETIMER_SYNCBUSY_CMD , LETIMER_SYNCBUSY_CTRL , LETIMER_Init_TypeDef::out0Pol , LETIMER_Init_TypeDef::out1Pol , LETIMER_Init_TypeDef::repMode , LETIMER_Init_TypeDef::rtcComp0Enable , LETIMER_Init_TypeDef::rtcComp1Enable , LETIMER_TypeDef::STATUS , LETIMER_TypeDef::SYNCBUSY , LETIMER_Init_TypeDef::topValue , LETIMER_Init_TypeDef::ufoa0 , and LETIMER_Init_TypeDef::ufoa1 .
Referenced by MIC_init() .
| __STATIC_INLINE void LETIMER_IntClear | ( | LETIMER_TypeDef * | 
           
            letimer,
           
           | 
         
| uint32_t | 
           
            flags
           
           | 
         ||
| ) | 
Clear one or more pending LETIMER interrupts.
- Parameters
 - 
         
[in] letimerPointer to LETIMER peripheral register block. [in] flagsPending LETIMER interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for the LETIMER module (LETIMER_IF_nnn).  
        Definition at line
        
         184
        
        of file
        
         em_letimer.h
        
        .
       
References LETIMER_TypeDef::IFC .
Referenced by LETIMER_Reset() .
| __STATIC_INLINE void LETIMER_IntDisable | ( | LETIMER_TypeDef * | 
           
            letimer,
           
           | 
         
| uint32_t | 
           
            flags
           
           | 
         ||
| ) | 
Disable one or more LETIMER interrupts.
- Parameters
 - 
         
[in] letimerPointer to LETIMER peripheral register block. [in] flagsLETIMER interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for the LETIMER module (LETIMER_IF_nnn).  
        Definition at line
        
         204
        
        of file
        
         em_letimer.h
        
        .
       
References LETIMER_TypeDef::IEN .
| __STATIC_INLINE void LETIMER_IntEnable | ( | LETIMER_TypeDef * | 
           
            letimer,
           
           | 
         
| uint32_t | 
           
            flags
           
           | 
         ||
| ) | 
Enable one or more LETIMER interrupts.
- Note
 - Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using LETIMER_IntClear() prior to enabling the interrupt.
 
- Parameters
 - 
         
[in] letimerPointer to the LETIMER peripheral register block. [in] flagsLETIMER interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for the LETIMER module (LETIMER_IF_nnn).  
        Definition at line
        
         225
        
        of file
        
         em_letimer.h
        
        .
       
References LETIMER_TypeDef::IEN .
| __STATIC_INLINE uint32_t LETIMER_IntGet | ( | LETIMER_TypeDef * | 
           
            letimer
           
           | 
          ) | 
Get pending LETIMER interrupt flags.
- Note
 - Event bits are not cleared by the use of this function.
 
- Parameters
 - 
         
[in] letimerPointer to LETIMER peripheral register block.  
- Returns
 - LETIMER interrupt sources pending. A bitwise logic OR combination of valid interrupt flags for the LETIMER module (LETIMER_IF_nnn).
 
        Definition at line
        
         244
        
        of file
        
         em_letimer.h
        
        .
       
References LETIMER_TypeDef::IF .
| __STATIC_INLINE uint32_t LETIMER_IntGetEnabled | ( | LETIMER_TypeDef * | 
           
            letimer
           
           | 
          ) | 
Get enabled and pending LETIMER interrupt flags.
Useful for handling more interrupt sources in the same interrupt handler.
- Note
 - Event bits are not cleared by the use of this function.
 
- Parameters
 - 
         
[in] letimerPointer to LETIMER peripheral register block.  
- Returns
 - 
         Pending and enabled LETIMER interrupt sources. Return value is the bitwise AND combination of
         
- the OR combination of enabled interrupt sources in LETIMER_IEN_nnn register (LETIMER_IEN_nnn) and
 - the OR combination of valid interrupt flags of the LETIMER module (LETIMER_IF_nnn).
 
 
        Definition at line
        
         270
        
        of file
        
         em_letimer.h
        
        .
       
References LETIMER_TypeDef::IEN , and LETIMER_TypeDef::IF .
| __STATIC_INLINE void LETIMER_IntSet | ( | LETIMER_TypeDef * | 
           
            letimer,
           
           | 
         
| uint32_t | 
           
            flags
           
           | 
         ||
| ) | 
Set one or more pending LETIMER interrupts from SW.
- Parameters
 - 
         
[in] letimerPointer to LETIMER peripheral register block. [in] flagsLETIMER interrupt sources to set to pending. Use a bitwise logic OR combination of valid interrupt flags for the LETIMER module (LETIMER_IF_nnn).  
        Definition at line
        
         293
        
        of file
        
         em_letimer.h
        
        .
       
References LETIMER_TypeDef::IFS .
| uint32_t LETIMER_RepeatGet | ( | LETIMER_TypeDef * | 
           
            letimer,
           
           | 
         
| unsigned int | 
           
            rep
           
           | 
         ||
| ) | 
Get the LETIMER repeat register value.
- Parameters
 - 
         
[in] letimerA pointer to the LETIMER peripheral register block. [in] repRepeat register to get, either 0 or 1.  
- Returns
 - Repeat register value, 0 if invalid register selected.
 
        Definition at line
        
         422
        
        of file
        
         em_letimer.c
        
        .
       
References LETIMER_TypeDef::REP0 , and LETIMER_TypeDef::REP1 .
| void LETIMER_RepeatSet | ( | LETIMER_TypeDef * | 
           
            letimer,
           
           | 
         
| unsigned int | 
           
            rep,
           
           | 
         ||
| uint32_t | 
           
            value
           
           | 
         ||
| ) | 
Set the LETIMER repeat counter register value.
- Note
 - The setting of a repeat counter register requires synchronization into the low-frequency domain. If the same register is modified before a previous update has completed, this function will stall until the previous synchronization has completed. This only applies to the Gecko Family. See comments in the LETIMER_Sync() internal function call.
 
- Parameters
 - 
         
[in] letimerA pointer to the LETIMER peripheral register block. [in] repRepeat counter register to set, either 0 or 1. [in] valueAn initialization value (<= 0x0000ffff).  
        Definition at line
        
         467
        
        of file
        
         em_letimer.c
        
        .
       
References _LETIMER_REP0_REP0_MASK , _LETIMER_REP0_REP0_SHIFT , LETIMER_SYNCBUSY_REP0 , LETIMER_SYNCBUSY_REP1 , LETIMER_TypeDef::REP0 , and LETIMER_TypeDef::REP1 .
Referenced by MIC_init() .
| void LETIMER_Reset | ( | LETIMER_TypeDef * | 
           
            letimer
           
           | 
          ) | 
Reset LETIMER to the same state that it was in after a hardware reset.
- Note
 - The ROUTE register is NOT reset by this function to allow for a centralized setup of this feature.
 
- Parameters
 - 
         
[in] letimerA pointer to the LETIMER peripheral register block.  
        Definition at line
        
         521
        
        of file
        
         em_letimer.c
        
        .
       
References _LETIMER_COMP0_RESETVALUE , _LETIMER_COMP1_RESETVALUE , _LETIMER_CTRL_RESETVALUE , _LETIMER_IEN_RESETVALUE , _LETIMER_IF_MASK , _LETIMER_REP0_RESETVALUE , _LETIMER_REP1_RESETVALUE , _LETIMER_SYNCBUSY_MASK , LETIMER_TypeDef::CMD , LETIMER_TypeDef::COMP0 , LETIMER_TypeDef::COMP1 , LETIMER_TypeDef::CTRL , LETIMER_TypeDef::IEN , LETIMER0 , LETIMER_CMD_CLEAR , LETIMER_CMD_CTO0 , LETIMER_CMD_CTO1 , LETIMER_CMD_STOP , LETIMER_FreezeEnable() , LETIMER_IntClear() , LETIMER_TypeDef::REP0 , and LETIMER_TypeDef::REP1 .
| __STATIC_INLINE uint32_t LETIMER_TopGet | ( | LETIMER_TypeDef * | 
           
            letimer
           
           | 
          ) | 
Get the current LETIMER top value.
- Parameters
 - 
         
[in] letimerA pointer to the LETIMER peripheral register block.  
- Returns
 - The top value. This will be a 16 bit value on series-0 and series-1 devices and a 24 bit value on series-2 devices.
 
        Definition at line
        
         321
        
        of file
        
         em_letimer.h
        
        .
       
References LETIMER_TypeDef::COMP0 .
| void LETIMER_TopSet | ( | LETIMER_TypeDef * | 
           
            letimer,
           
           | 
         
| uint32_t | 
           
            value
           
           | 
         ||
| ) | 
Set the LETIMER top value.
- Note
 - The LETIMER is a down-counter, so when the counter reaches 0 then the top value will be loaded into the counter. This function can be used to set the top value.
 
If the LETIMER is not already configured to use a top value then this function will enable that functionality for the user.
- Parameters
 - 
         
[in] letimerA pointer to the LETIMER peripheral register block. [in] valueThe top value. This can be a 16 bit value on series-0 and series-1 devices and a 24 bit value on series-2 devices.  
        Definition at line
        
         591
        
        of file
        
         em_letimer.c
        
        .
       
References LETIMER_TypeDef::CTRL , LETIMER_CompareSet() , LETIMER_CTRL_COMP0TOP , and LETIMER_SyncWait() .