em_usbxpress_callback.c File Reference
Contains call-back functions from the EFM32 USB Library.
License
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.
       Definition in file
       
        em_usbxpress_callback.c
       
       .
      
       #include <stddef.h>
      
      
       #include "
       
        em_usbxpress_internal.h
       
       "
      
      
       #include "
       
        em_usbxpress_descriptors.h
       
       "
      
      
       #include "
       
        em_usbxpress.h
       
       "
      
      
| Functions | |
| static uint8_t usbxpressPartNumber | SL_ATTRIBUTE_ALIGN (4) | 
| USBXpress Part Number. | |
| void | USBX_DeviceStateChangeCb ( USBD_State_TypeDef oldState, USBD_State_TypeDef newState) | 
| USB device state change call-back. | |
| int | USBX_inXferCompleteCb ( USB_Status_TypeDef status, uint16_t xferred, uint16_t remaining) | 
| USBXpress IN Endpoint Transfer Complete Callback. | |
| int | USBX_outXferCompleteCb ( USB_Status_TypeDef status, uint16_t xferred, uint16_t remaining) | 
| USBXpress OUT Endpoint Transfer Complete Callback. | |
| void | USBX_ResetCb (void) | 
| USB Reset call-back. | |
| int | USBX_SetupCmdCb (const USB_Setup_TypeDef *setup) | 
| USB setup command call-back. | |
| Variables | |
| uint8_t | USBXCORE_overflowBuffer [] | 
| bool | USBXCORE_rxOverflowPacketAvailable | 
| Boolean indicating if data was received while expecting a ZLP. | |
| uint32_t | USBXCORE_rxOverflowPacketSize | 
| Size of Rx Overflow Packet. | |
| bool | USBXCORE_zlpActive | 
| Boolean indicating whether a ZLP read is active. | |
Function Documentation
| 
 | static | 
USBXpress Part Number.
USBXpress Library Version.
| void USBX_DeviceStateChangeCb | ( | USBD_State_TypeDef | 
            oldState,
            | 
| USBD_State_TypeDef | 
            newState
            | ||
| ) | 
USB device state change call-back.
Set new state and jump to user API call-back.
        Definition at line
        
         73
        
        of file
        
         em_usbxpress_callback.c
        
        .
       
        References
        
         APIEA_GIE
        
        ,
        
         USBD_STATE_CONFIGURED
        
        ,
        
         USBD_STATE_SUSPENDED
        
        ,
        
         USBX_DEV_CONFIGURED
        
        ,
        
         USBX_DEV_SUSPEND
        
        ,
        
         USBX_jumpCallback()
        
        ,
        
         USBXCORE_apiEa
        
        ,
        
         USBXCORE_apiIntValue
        
        , and
        
         USBXCORE_resetState()
        
        .
       
Referenced by USBX_init() .
| int USBX_inXferCompleteCb | ( | USB_Status_TypeDef | 
            status,
            | 
| uint16_t | 
            xferred,
            | ||
| uint16_t | 
            remaining
            | ||
| ) | 
USBXpress IN Endpoint Transfer Complete Callback.
Gets the number of IN bytes transferred and passes them to the user API call-back.
        Definition at line
        
         244
        
        of file
        
         em_usbxpress_callback.c
        
        .
       
        References
        
         APIEA_GIE
        
        ,
        
         USB_FS_BULK_EP_MAXSIZE
        
        ,
        
         USB_STATUS_OK
        
        ,
        
         USBD_Write()
        
        ,
        
         USBX_jumpCallback()
        
        ,
        
         USBX_TX_COMPLETE
        
        ,
        
         USBXCORE_apiEa
        
        ,
        
         USBXCORE_apiIntValue
        
        ,
        
         USBXCORE_byteCountInPtr
        
        , and
        
         USBXCORE_writeSize
        
        .
       
Referenced by USBX_blockWrite() .
| int USBX_outXferCompleteCb | ( | USB_Status_TypeDef | 
            status,
            | 
| uint16_t | 
            xferred,
            | ||
| uint16_t | 
            remaining
            | ||
| ) | 
USBXpress OUT Endpoint Transfer Complete Callback.
Gets the number of OUT bytes transferred and passes them to the user API call-back.
        Definition at line
        
         284
        
        of file
        
         em_usbxpress_callback.c
        
        .
       
        References
        
         APIEA_GIE
        
        ,
        
         USB_STATUS_OK
        
        ,
        
         USBD_Read()
        
        ,
        
         USBX_jumpCallback()
        
        ,
        
         USBX_RX_COMPLETE
        
        ,
        
         USBX_RX_OVERRUN
        
        ,
        
         USBXCORE_apiEa
        
        ,
        
         USBXCORE_apiIntValue
        
        ,
        
         USBXCORE_byteCountOutPtr
        
        , and
        
         USBXCORE_readSize
        
        .
       
Referenced by USBX_blockRead() .
| void USBX_ResetCb | ( | void | 
            | ) | 
USB Reset call-back.
Jump to user API RESET call-back.
        Definition at line
        
         56
        
        of file
        
         em_usbxpress_callback.c
        
        .
       
        References
        
         APIEA_GIE
        
        ,
        
         USBX_jumpCallback()
        
        ,
        
         USBX_RESET
        
        ,
        
         USBXCORE_apiEa
        
        ,
        
         USBXCORE_apiIntValue
        
        , and
        
         USBXCORE_resetState()
        
        .
       
Referenced by USBX_init() .
| int USBX_SetupCmdCb | ( | const USB_Setup_TypeDef * | 
            setup
            | ) | 
USB setup command call-back.
If the setup command is a vendor request, pass to the USB command request parsing routine and acknowledge. Otherwise ignore the request.
        Definition at line
        
         103
        
        of file
        
         em_usbxpress_callback.c
        
        .
       
        References
        
         APIEA_GIE
        
        ,
        
         APIEA_GIE_TEMP
        
        ,
        
         USB_Setup_TypeDef::bmRequestType
        
        ,
        
         USB_Setup_TypeDef::bRequest
        
        ,
        
         EXT_COMP_DESC_SIZE
        
        ,
        
         EXT_COMP_VENDOR_CODE
        
        ,
        
         FEATURE_EXTENDED_COMPATIBILITY_ID
        
        ,
        
         FEATURE_EXTENDED_PROPERTIES_ID
        
        ,
        
         GET_DESCRIPTOR
        
        ,
        
         PROPERTIES_DESCRIPTOR_SIZE
        
        ,
        
         SI_CP210X_GET_PART_NUMBER
        
        ,
        
         SI_CP210X_REQUEST
        
        ,
        
         SI_USBXPRESS_CLEAR_TO_SEND
        
        ,
        
         SI_USBXPRESS_FLUSH_BUFFERS
        
        ,
        
         SI_USBXPRESS_GET_VERSION
        
        ,
        
         SI_USBXPRESS_NOT_CLEAR_TO_SEND
        
        ,
        
         SI_USBXPRESS_REQUEST
        
        ,
        
         USB_Setup_TypeDef::Type
        
        ,
        
         USB_SETUP_DIR_D2H
        
        ,
        
         USB_SETUP_RECIPIENT_DEVICE
        
        ,
        
         USB_SETUP_RECIPIENT_INTERFACE
        
        ,
        
         USB_SETUP_TYPE_STANDARD
        
        ,
        
         USB_SETUP_TYPE_VENDOR
        
        ,
        
         USB_SETUP_TYPE_VENDOR_MASK
        
        ,
        
         USB_STATUS_OK
        
        ,
        
         USB_STATUS_REQ_UNHANDLED
        
        ,
        
         USB_STRING_DESCRIPTOR
        
        ,
        
         USBD_AbortTransfer()
        
        ,
        
         USBD_Write()
        
        ,
        
         USBX_DEV_CLOSE
        
        ,
        
         USBX_DEV_OPEN
        
        ,
        
         USBX_FIFO_PURGE
        
        ,
        
         USBX_jumpCallback()
        
        ,
        
         USBXCORE_apiEa
        
        ,
        
         USBXCORE_apiIntValue
        
        ,
        
         USBXCORE_resetState()
        
        ,
        
         USB_Setup_TypeDef::wIndex
        
        ,
        
         USB_Setup_TypeDef::wLength
        
        , and
        
         USB_Setup_TypeDef::wValue
        
        .
       
Referenced by USBX_init() .