retargettextdisplay.c File Reference
Provide stdio retargeting to text display interface.
License
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.
       Definition in file
       
        retargettextdisplay.c
       
       .
      
       #include <stdio.h>
      
      
       #include <stdint.h>
      
      
       #include "
       
        displayconfigall.h
       
       "
      
      
       #include "
       
        display.h
       
       "
      
      
       #include "
       
        textdisplay.h
       
       "
      
      
       #include "
       
        retargettextdisplay.h
       
       "
      
      
| Functions | |
| int | RETARGET_ReadChar (void) | 
| Receive a byte No input method from the text display is possible, thus we always return -1. | |
| EMSTATUS | RETARGET_TextDisplayInit (void) | 
| Initialize/retarget a TEXTDISPLAY device to receivie stdout(put). | |
| int | RETARGET_WriteChar (char c) | 
| Write a single byte to the text display. | |
| EMSTATUS | RETARGET_WriteString (char *str) | 
| Write a string of characters to the RETARGET text display device. | |
Function Documentation
| int RETARGET_ReadChar | ( | void | 
            | ) | 
Receive a byte No input method from the text display is possible, thus we always return -1.
- Returns
- -1 on failure
        Definition at line
        
         80
        
        of file
        
         retargettextdisplay.c
        
        .
       
| int RETARGET_WriteChar | ( | char | 
            c
            | ) | 
Write a single byte to the text display.
- Parameters
- 
         cCharacter to write 
- Returns
- Printed character if text display is initialized. -1 if text display is not initialized.
        Definition at line
        
         93
        
        of file
        
         retargettextdisplay.c
        
        .
       
References TEXTDISPLAY_WriteChar() .