cal_ref_t Struct Reference
Structure Definition for calref array.
       Definition at line
       
        780
       
       of file
       
        si114x_functions.c
       
       .
      
         Data Fields | 
       |
| uint32_t | ledi_65ma | 
| uint32_t | lirpd_adchi_irled | 
| uint32_t | sirpd_adchi_irled | 
| uint32_t | sirpd_adclo_irled | 
| uint32_t | sirpd_adclo_whled | 
| uint8_t | ucoef [4] | 
| uint32_t | vispd_adchi_whled | 
| uint32_t | vispd_adclo_whled | 
Field Documentation
| uint32_t cal_ref_t::ledi_65ma | 
LED Current Ratio at 65 mA
        Definition at line
        
         787
        
        of file
        
         si114x_functions.c
        
        .
       
| uint32_t cal_ref_t::lirpd_adchi_irled | 
Large IR PD gain, IR LED, Hi ADC Range
        Definition at line
        
         786
        
        of file
        
         si114x_functions.c
        
        .
       
| uint32_t cal_ref_t::sirpd_adchi_irled | 
Small IR PD gain, IR LED, Hi ADC Range
        Definition at line
        
         781
        
        of file
        
         si114x_functions.c
        
        .
       
| uint32_t cal_ref_t::sirpd_adclo_irled | 
Small IR PD gain, IR LED, Lo ADC Range
        Definition at line
        
         782
        
        of file
        
         si114x_functions.c
        
        .
       
| uint32_t cal_ref_t::sirpd_adclo_whled | 
Small IR PD gain, White LED, Lo ADC Range
        Definition at line
        
         783
        
        of file
        
         si114x_functions.c
        
        .
       
| uint8_t cal_ref_t::ucoef[4] | 
UV Coefficient Storage
        Definition at line
        
         788
        
        of file
        
         si114x_functions.c
        
        .
       
Referenced by si114x_get_calibration() .
| uint32_t cal_ref_t::vispd_adchi_whled | 
VIS PD gain, White LED, Lo ADC Range
        Definition at line
        
         784
        
        of file
        
         si114x_functions.c
        
        .
       
| uint32_t cal_ref_t::vispd_adclo_whled | 
VIS PD gain, White LED, Lo ADC Range
        Definition at line
        
         785
        
        of file
        
         si114x_functions.c
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/cygwin/home/caamunds/work/super/hardware/kit/common/drivers/
       
si114x_functions.c