LFN parent parameter set.
Public Attributes#
uint8_t
Number of broadcast LFN Pan Config retries when LFN Version is incremented Referred to as LFN_MAINTAIN_PARENT_TIME in FAN TPS 1.1.
uint8_t
Reserved, set to zero.
Public Attribute Documentation#
lfn_lpc_retry_count#
uint8_t sl_wisun_br_params_lfn_parent_s::lfn_lpc_retry_count
Number of broadcast LFN Pan Config retries when LFN Version is incremented Referred to as LFN_MAINTAIN_PARENT_TIME in FAN TPS 1.1.
Definition at line
160
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/border_router/sl_wisun_br_connection_params_api.h
reserved#
uint8_t sl_wisun_br_params_lfn_parent_s::reserved[3]
Reserved, set to zero.
Definition at line
162
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/border_router/sl_wisun_br_connection_params_api.h