Adaptive rate algorithm rate stats.
Public Attributes#
uint16_t
Number of tx without acknowledgement.
uint32_t
Frame tx time.
int8_t
Indicates if the rate can be probed.
uint8_t
Reserved, set to zero.
uint32_t
Number of times the rate was selected.
uint8_t
Number of times this rate was skipped.
uint16_t
Number of successful transmissions.
float
Estimated chance of success.
float
Estimated troughput in kb/s.
Public Attribute Documentation#
fail_count#
uint16_t sl_wisun_rate_stats_t::fail_count
Number of tx without acknowledgement.
Definition at line
851
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
frame_duration_us#
uint32_t sl_wisun_rate_stats_t::frame_duration_us
Frame tx time.
Definition at line
841
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
probe_limit#
int8_t sl_wisun_rate_stats_t::probe_limit
Indicates if the rate can be probed.
Definition at line
855
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
reserved#
uint8_t sl_wisun_rate_stats_t::reserved[2]
Reserved, set to zero.
Definition at line
857
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
sample_count#
uint32_t sl_wisun_rate_stats_t::sample_count
Number of times the rate was selected.
Definition at line
843
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
skipped_sample_count#
uint8_t sl_wisun_rate_stats_t::skipped_sample_count
Number of times this rate was skipped.
Definition at line
853
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
success_count#
uint16_t sl_wisun_rate_stats_t::success_count
Number of successful transmissions.
Definition at line
849
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
success_probability#
float sl_wisun_rate_stats_t::success_probability
Estimated chance of success.
Definition at line
845
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
throughput#
float sl_wisun_rate_stats_t::throughput
Estimated troughput in kb/s.
Definition at line
847
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h