MPL parameter set.
Public Attributes#
uint8_t
Reserved, set to zero.
uint16_t
MPL seed set entry lifetime.
Warning: MPL parameters may be overwritten for border router MPL trickle timer.
uint8_t
MPL trickle timer expirations.
Public Attribute Documentation#
reserved#
uint8_t sl_wisun_br_params_mpl_s::reserved
Reserved, set to zero.
Definition at line
146
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/border_router/sl_wisun_br_connection_params_api.h
seed_set_entry_lifetime_s#
uint16_t sl_wisun_br_params_mpl_s::seed_set_entry_lifetime_s
MPL seed set entry lifetime.
Definition at line
142
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/border_router/sl_wisun_br_connection_params_api.h
trickle#
sl_wisun_trickle_params_t sl_wisun_br_params_mpl_s::trickle
Warning: MPL parameters may be overwritten for border router MPL trickle timer.
Definition at line
140
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/border_router/sl_wisun_br_connection_params_api.h
trickle_expirations#
uint8_t sl_wisun_br_params_mpl_s::trickle_expirations
MPL trickle timer expirations.
Definition at line
144
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/border_router/sl_wisun_br_connection_params_api.h