MAC statistics.
Public Attributes#
Number of successfully received broadcast MAC frames.
Number of transmitted broadcast MAC frames.
Number of MAC CCA attempts.
Number of failed MAC transmissions due to CCA.
Number of retried MAC transmissions.
Amount of successfully received MAC data in bytes. FCS is not included.
Number of successfully received MAC frames.
Number of successfully received MAC frames discarded during processing.
Number of successfully received MAC frames using mode_switch.
Number of failed reception using mode switch (no data after PHR or MDR Command).
Amount of transmitted MAC data in bytes. FCS is not included.
Number of transmitted MAC frames.
Number of failed MAC transmissions.
Number of transmitted MAC frames using mode switch.
Number of failed MAC frames transmission using mode switch.
Highest number of frames in the MAC transmission queue.
Current number of frames in the MAC transmission queue.
Public Attribute Documentation#
bc_rx_count#
uint32_t sl_wisun_statistics_mac_t::bc_rx_count
Number of successfully received broadcast MAC frames.
366
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
bc_tx_count#
uint32_t sl_wisun_statistics_mac_t::bc_tx_count
Number of transmitted broadcast MAC frames.
368
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
cca_attempts_count#
uint32_t sl_wisun_statistics_mac_t::cca_attempts_count
Number of MAC CCA attempts.
380
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
failed_cca_count#
uint32_t sl_wisun_statistics_mac_t::failed_cca_count
Number of failed MAC transmissions due to CCA.
382
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
retry_count#
uint32_t sl_wisun_statistics_mac_t::retry_count
Number of retried MAC transmissions.
378
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
rx_bytes#
uint32_t sl_wisun_statistics_mac_t::rx_bytes
Amount of successfully received MAC data in bytes. FCS is not included.
374
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
rx_count#
uint32_t sl_wisun_statistics_mac_t::rx_count
Number of successfully received MAC frames.
362
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
rx_drop_count#
uint32_t sl_wisun_statistics_mac_t::rx_drop_count
Number of successfully received MAC frames discarded during processing.
370
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
rx_ms_count#
uint32_t sl_wisun_statistics_mac_t::rx_ms_count
Number of successfully received MAC frames using mode_switch.
384
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
rx_ms_failed_count#
uint32_t sl_wisun_statistics_mac_t::rx_ms_failed_count
Number of failed reception using mode switch (no data after PHR or MDR Command).
388
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
tx_bytes#
uint32_t sl_wisun_statistics_mac_t::tx_bytes
Amount of transmitted MAC data in bytes. FCS is not included.
372
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
tx_count#
uint32_t sl_wisun_statistics_mac_t::tx_count
Number of transmitted MAC frames.
364
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
tx_failed_count#
uint32_t sl_wisun_statistics_mac_t::tx_failed_count
Number of failed MAC transmissions.
376
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
tx_ms_count#
uint32_t sl_wisun_statistics_mac_t::tx_ms_count
Number of transmitted MAC frames using mode switch.
386
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
tx_ms_failed_count#
uint32_t sl_wisun_statistics_mac_t::tx_ms_failed_count
Number of failed MAC frames transmission using mode switch.
390
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
tx_queue_peak#
uint16_t sl_wisun_statistics_mac_t::tx_queue_peak
Highest number of frames in the MAC transmission queue.
360
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
tx_queue_size#
uint16_t sl_wisun_statistics_mac_t::tx_queue_size
Current number of frames in the MAC transmission queue.
358
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h