Wi-SUN Message API common header.
Public Attributes#
uint8_t
ID (request, confirmation, indication) of the message.
uint8_t
Processing metadata for the message.
uint16_t
Total length of the message in bytes, this field included.
Public Attribute Documentation#
id#
uint8_t sl_wisun_msg_header_t::id
ID (request, confirmation, indication) of the message.
Definition at line
339
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
info#
uint8_t sl_wisun_msg_header_t::info
Processing metadata for the message.
Definition at line
341
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
length#
uint16_t sl_wisun_msg_header_t::length
Total length of the message in bytes, this field included.
Definition at line
337
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h