RPL neighbor information.
Public Attributes#
Measured ETX value if known (0xffff if unknown)
ULA/GUA address (unspecified address :: if unknown)
Indicate if the device is an LFN. 1 = LFN, 0 = FFN.
Indicate if the neighbor supports MAC mode switch.
Remaining lifetime (Link lifetime for parents, EARO lifetime for children) in seconds.
Link-local address.
MAC RX packet count.
MAC TX packet count.
MAC TX failed count.
MAC TX packet count using mode switch.
MAC TX failed count using mode switch.
Number devices connected to Border Router.
Number of PhyModeId supported.
List of phy_mode_id_count PhyModeId.
ETX to Border Router.
RPL Rank value for parents (0xffff if unknown or child)
Parent RSSI In measured RSSI value (0xff if unknown) Calculated using EWMA specified by Wi-SUN from range of -174 (0) to +80 (254) dBm.
Parent RSSI Out measured RSSI value (0xff if unknown) Calculated using EWMA specified by Wi-SUN from range of -174 (0) to +80 (254) dBm.
RSSI of the last received packet in integer dBm. */.
Neighbor type (sl_wisun_neighbor_type_t)
Public Attribute Documentation#
etx#
uint16_t sl_wisun_neighbor_info_t::etx
Measured ETX value if known (0xffff if unknown)
813
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
global_address#
in6_addr_t sl_wisun_neighbor_info_t::global_address
ULA/GUA address (unspecified address :: if unknown)
795
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
is_lfn#
uint8_t sl_wisun_neighbor_info_t::is_lfn
Indicate if the device is an LFN. 1 = LFN, 0 = FFN.
827
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
is_mdr_command_capable#
uint8_t sl_wisun_neighbor_info_t::is_mdr_command_capable
Indicate if the neighbor supports MAC mode switch.
833
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
lifetime#
uint32_t sl_wisun_neighbor_info_t::lifetime
Remaining lifetime (Link lifetime for parents, EARO lifetime for children) in seconds.
799
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
link_local_address#
in6_addr_t sl_wisun_neighbor_info_t::link_local_address
Link-local address.
793
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
mac_rx_count#
uint32_t sl_wisun_neighbor_info_t::mac_rx_count
MAC RX packet count.
809
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
mac_tx_count#
uint32_t sl_wisun_neighbor_info_t::mac_tx_count
MAC TX packet count.
801
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
mac_tx_failed_count#
uint32_t sl_wisun_neighbor_info_t::mac_tx_failed_count
MAC TX failed count.
803
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
mac_tx_ms_count#
uint32_t sl_wisun_neighbor_info_t::mac_tx_ms_count
MAC TX packet count using mode switch.
805
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
mac_tx_ms_failed_count#
uint32_t sl_wisun_neighbor_info_t::mac_tx_ms_failed_count
MAC TX failed count using mode switch.
807
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
pan_size#
uint16_t sl_wisun_neighbor_info_t::pan_size
Number devices connected to Border Router.
817
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
phy_mode_id_count#
uint8_t sl_wisun_neighbor_info_t::phy_mode_id_count
Number of PhyModeId supported.
829
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
phy_mode_ids#
uint8_t sl_wisun_neighbor_info_t::phy_mode_ids[SL_WISUN_MAX_PHY_MODE_ID_COUNT]
List of phy_mode_id_count PhyModeId.
831
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
routing_cost#
uint16_t sl_wisun_neighbor_info_t::routing_cost
ETX to Border Router.
815
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
rpl_rank#
uint16_t sl_wisun_neighbor_info_t::rpl_rank
RPL Rank value for parents (0xffff if unknown or child)
811
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
rsl_in#
uint8_t sl_wisun_neighbor_info_t::rsl_in
Parent RSSI In measured RSSI value (0xff if unknown) Calculated using EWMA specified by Wi-SUN from range of -174 (0) to +80 (254) dBm.
823
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
rsl_out#
uint8_t sl_wisun_neighbor_info_t::rsl_out
Parent RSSI Out measured RSSI value (0xff if unknown) Calculated using EWMA specified by Wi-SUN from range of -174 (0) to +80 (254) dBm.
820
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
rssi#
int8_t sl_wisun_neighbor_info_t::rssi
RSSI of the last received packet in integer dBm. */.
825
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
type#
uint32_t sl_wisun_neighbor_info_t::type
Neighbor type (sl_wisun_neighbor_type_t)
797
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h