RPL parameter set.

Public Attributes#

uint16_t

Amount of time a parent should retain a registered GUA/ULA (seconds)

uint8_t

RPL max candidate parents.

uint16_t

RPL first DIS maximum delay (seconds)

uint16_t

RPL DIS maximum delay (seconds)

uint16_t

Maximum period of NS probes used to get samples for ETX calculation (seconds)

uint8_t

Number of samples used to calculate ETX during join state 4.

uint8_t

Number of samples used to refresh ETX.

uint16_t

Delay for preferred parent selection after first DIO reception (seconds)

uint8_t

RPL max parents.

Public Attribute Documentation#

address_registration_lifetime_s#

uint16_t sl_wisun_params_rpl_s::address_registration_lifetime_s

Amount of time a parent should retain a registered GUA/ULA (seconds)


Definition at line 210 of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h

candidate_parents_max#

uint8_t sl_wisun_params_rpl_s::candidate_parents_max

RPL max candidate parents.


Definition at line 216 of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h

dis_max_delay_first_s#

uint16_t sl_wisun_params_rpl_s::dis_max_delay_first_s

RPL first DIS maximum delay (seconds)


Definition at line 202 of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h

dis_max_delay_s#

uint16_t sl_wisun_params_rpl_s::dis_max_delay_s

RPL DIS maximum delay (seconds)


Definition at line 204 of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h

etx_probe_period_max_s#

uint16_t sl_wisun_params_rpl_s::etx_probe_period_max_s

Maximum period of NS probes used to get samples for ETX calculation (seconds)


Definition at line 208 of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h

etx_samples_init#

uint8_t sl_wisun_params_rpl_s::etx_samples_init

Number of samples used to calculate ETX during join state 4.


Definition at line 212 of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h

etx_samples_refresh#

uint8_t sl_wisun_params_rpl_s::etx_samples_refresh

Number of samples used to refresh ETX.


Definition at line 214 of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h

init_parent_selection_s#

uint16_t sl_wisun_params_rpl_s::init_parent_selection_s

Delay for preferred parent selection after first DIO reception (seconds)


Definition at line 206 of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h

parents_max#

uint8_t sl_wisun_params_rpl_s::parents_max

RPL max parents.


Definition at line 218 of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h