LFN network parameters.

Public Attributes#

uint8_t

Duration for which an LFN waits for a registration confirmation (minutes).

uint16_t

Address registration lifetime (IPv6 lease duration) the LFN requires to the Border Router (minutes).

uint8_t

Reserved, set to zero.

Public Attribute Documentation#

lfn_na_wait_duration_m#

uint8_t sl_wisun_lfn_params_network_t::lfn_na_wait_duration_m

Duration for which an LFN waits for a registration confirmation (minutes).

This value is administratively configured and should be consistent throughout the network. Make sure that the value is equal to or greather than the corresponding field on FFNs. Specification range [30, 120] (set lower for test purposes)


Definition at line 93 of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h

lfn_registration_lifetime_m#

uint16_t sl_wisun_lfn_params_network_t::lfn_registration_lifetime_m

Address registration lifetime (IPv6 lease duration) the LFN requires to the Border Router (minutes).

Specification range [1440, 5040]


Definition at line 87 of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h

reserved#

uint8_t sl_wisun_lfn_params_network_t::reserved

Reserved, set to zero.


Definition at line 95 of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h