RPL parameter set.
Public Attributes#
Reserved, set to zero.
RPL allowable increase in rank in support of local repair RFC 6550 6.7.6.
RPL default lifetime for routes (lifetime units) RFC6550 6.7.6.
RPL default lifetime unit RFC6550 6.7.6.
RPL trickle Imax (DIOIntervalDoublings)
RPL trickle Imin equals (2^rpl_dio_interval_min) ms.
RPL trickle k DIORedundancyConstant.
RPL MinHopRankIncrease RFC6550 3.5.1.
Public Attribute Documentation#
reserved#
uint8_t sl_wisun_br_params_rpl_s::reserved[2]
Reserved, set to zero.
126
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/border_router/sl_wisun_br_connection_params_api.h
rpl_dag_max_rank_increase#
uint16_t sl_wisun_br_params_rpl_s::rpl_dag_max_rank_increase
RPL allowable increase in rank in support of local repair RFC 6550 6.7.6.
114
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/border_router/sl_wisun_br_connection_params_api.h
rpl_default_lifetime#
uint8_t sl_wisun_br_params_rpl_s::rpl_default_lifetime
RPL default lifetime for routes (lifetime units) RFC6550 6.7.6.
124
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/border_router/sl_wisun_br_connection_params_api.h
rpl_default_lifetime_unit#
uint16_t sl_wisun_br_params_rpl_s::rpl_default_lifetime_unit
RPL default lifetime unit RFC6550 6.7.6.
116
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/border_router/sl_wisun_br_connection_params_api.h
rpl_dio_interval_doublings#
uint8_t sl_wisun_br_params_rpl_s::rpl_dio_interval_doublings
RPL trickle Imax (DIOIntervalDoublings)
120
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/border_router/sl_wisun_br_connection_params_api.h
rpl_dio_interval_min#
uint8_t sl_wisun_br_params_rpl_s::rpl_dio_interval_min
RPL trickle Imin equals (2^rpl_dio_interval_min) ms.
118
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/border_router/sl_wisun_br_connection_params_api.h
rpl_dio_redundancy_constant#
uint8_t sl_wisun_br_params_rpl_s::rpl_dio_redundancy_constant
RPL trickle k DIORedundancyConstant.
122
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/border_router/sl_wisun_br_connection_params_api.h
rpl_min_hop_rank_increase#
uint16_t sl_wisun_br_params_rpl_s::rpl_min_hop_rank_increase
RPL MinHopRankIncrease RFC6550 3.5.1.
112
of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/protocol/wisun/stack/inc/border_router/sl_wisun_br_connection_params_api.h