You are viewing documentation for version:7.24.2PDFController API. Public Attributes#void(*Handlenode_id_tSucNodeIdPlaceholder for callback function Will be returned with transmit status Allows application to recognize frames. boolbSucEnableboolbTxLowPoweruint8_tCapabilitiesPublic Attribute Documentation#Handle#void(* SSetSucNodeId::Handle) (void)SucNodeId#node_id_t SSetSucNodeId::SucNodeIdPlaceholder for callback function Will be returned with transmit status Allows application to recognize frames. bSucEnable#bool SSetSucNodeId::bSucEnablebTxLowPower#bool SSetSucNodeId::bTxLowPowerCapabilities#uint8_t SSetSucNodeId::Capabilities