Data point descriptor. Compact attribute, Multi sensor or Generic switch feature uses this as descriptor to interpret the incoming data from the GPD. This descriptor is set up at the sink during the commissioning.

Public Attribute Documentation#

nbAttrRecord#

uint8_t EmberGpDataPointDescriptor::nbAttrRecord

Number of attribute records


Definition at line 624 of file stack/include/gp-types.h

clientServer#

uint8_t EmberGpDataPointDescriptor::clientServer

Client or Server flag


Definition at line 626 of file stack/include/gp-types.h

ManIdPresent#

uint8_t EmberGpDataPointDescriptor::ManIdPresent

Manufacture ID present


Definition at line 628 of file stack/include/gp-types.h

datapointOptions#

uint8_t EmberGpDataPointDescriptor::datapointOptions

Data point options


Definition at line 630 of file stack/include/gp-types.h

clusterID#

uint16_t EmberGpDataPointDescriptor::clusterID

Cluster ID


Definition at line 632 of file stack/include/gp-types.h

manufacturerID#

uint16_t EmberGpDataPointDescriptor::manufacturerID

Manufacture ID


Definition at line 634 of file stack/include/gp-types.h

attrRecord#

EmberGpAttributeRecord EmberGpDataPointDescriptor::attrRecord

Attribute Record


Definition at line 636 of file stack/include/gp-types.h