MN Price Passthrough Client/Server#
API and Callbacks for the MN Price Passthrough Cluster Client/Server Component.
This component demonstrates the capabilities of the multi-network support. The component acts as a Price cluster client on one network and a Price cluster server on another network. As a client, it periodically polls a remote server for pricing information and then stores the data locally. As a server, it makes that pricing information available to clients, thereby proxying the data between networks.
Functions#
void
sli_zigbee_af_mn_price_passthrough_routing_setup(sl_802154_short_addr_t fwdId, uint8_t fwdEndpoint, uint8_t esiEndpoint)
Function Documentation#
sli_zigbee_af_mn_price_passthrough_start_poll_and_forward#
void sli_zigbee_af_mn_price_passthrough_start_poll_and_forward (void )
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
sli_zigbee_af_mn_price_passthrough_stop_poll_and_forward#
void sli_zigbee_af_mn_price_passthrough_stop_poll_and_forward (void )
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
sli_zigbee_af_mn_price_passthrough_routing_setup#
void sli_zigbee_af_mn_price_passthrough_routing_setup (sl_802154_short_addr_t fwdId, uint8_t fwdEndpoint, uint8_t esiEndpoint)
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_802154_short_addr_t | N/A | fwdId | |
| uint8_t | N/A | fwdEndpoint | |
| uint8_t | N/A | esiEndpoint | 
sli_zigbee_af_mn_price_passthrough_print_current_price#
void sli_zigbee_af_mn_price_passthrough_print_current_price (void )
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A |