Standalone Bootloader Common#

API and Callbacks for the Standalone Bootloader Common Component.

Code common to both the client and server of the Silicon Labs standalone bootload protocol.

Modules#

Bootloader Protocol

API#

uint8_t

Make bootloader header.

sl_zigbee_af_standalone_bootloader_common_send_message(bool isBroadcast, sl_802154_long_addr_t targetEui, uint8_t length, uint8_t *message)

Send message.

bool

Check incoming message.

Macros#

#define
BOOTLOAD_OTA_SIZE 64
#define
MAX_BOOTLOAD_MESSAGE_SIZE (BOOTLOAD_OTA_SIZE + 6)
#define
BOOTLOAD_PROTOCOL_VERSION 1
#define
CHALLENGE_REQUEST_VERSION 0x01
#define
BOOTLOAD_MESSAGE_OVERHEAD 2
#define
OFFSET_VERSION 0
#define
OFFSET_MESSAGE_TYPE 1
#define
OFFSET_DEVICE_TYPE 2
#define
OFFSET_BLOCK_NUMBER 2
#define
OFFSET_ERROR_TYPE 2
#define
OFFSET_BLOCK_NUMBER_CHECK 3
#define
OFFSET_ERROR_BLOCK 3
#define
OFFSET_IMAGE_CONTENT 4
#define
QUERY_RESPONSE_LENGTH (BOOTLOAD_MESSAGE_OVERHEAD + 11)
#define
QRESP_OFFSET_BL_ACTIVE 2
#define
QRESP_OFFSET_MFG_ID 3
#define
QRESP_OFFSET_HARDWARE_TAG 5
#define
QRESP_OFFSET_BL_CAPS 21
#define
QRESP_OFFSET_PLATFORM 22
#define
QRESP_OFFSET_MICRO 23
#define
QRESP_OFFSET_PHY 24
#define
QRESP_OFFSET_BL_VERSION 25
#define
OFFSET_MFG_ID 2
#define
OFFSET_HARDWARE_TAG 4
#define
OFFSET_AUTH_CHALLENGE 2
#define
OFFSET_AUTH_RESPONSE 2
#define
XMODEM_QUERY 0x51
#define
XMODEM_QRESP 0x52
#define
XMODEM_CC 0x03
#define
XMODEM_LAUNCH_REQUEST 0x4c
#define
XMODEM_AUTH_CHALLENGE 0x63
#define
XMODEM_AUTH_RESPONSE 0x72
#define
BOOTLOAD_AUTH_COMMON_SIZE 16
#define
BOOTLOAD_AUTH_CHALLENGE_SIZE BOOTLOAD_AUTH_COMMON_SIZE
#define
BOOTLOAD_AUTH_RESPONSE_SIZE BOOTLOAD_AUTH_COMMON_SIZE
#define
QUERY_REQUEST_LENGTH (BOOTLOAD_MESSAGE_OVERHEAD)
#define
LAUNCH_REQUEST_LENGTH (BOOTLOAD_MESSAGE_OVERHEAD + 18)
#define
XMODEM_AUTH_CHALLENGE_LENGTH (BOOTLOAD_MESSAGE_OVERHEAD + 15)
#define
XMODEM_AUTH_CHALLENGE_REQUEST_INDEX (BOOTLOAD_MESSAGE_OVERHEAD)
#define
XMODEM_AUTH_RESPONSE_LENGTH (BOOTLOAD_MESSAGE_OVERHEAD + 16)
#define
bootloadPrintln (...)
#define
bootloadPrint (...)

API Documentation#

sl_zigbee_af_standalone_bootloader_common_make_header#

uint8_t sl_zigbee_af_standalone_bootloader_common_make_header (uint8_t * message, uint8_t type)

Make bootloader header.

Parameters
TypeDirectionArgument NameDescription
uint8_t *N/Amessage

Ver.: always

uint8_tN/Atype

Ver.: always

Returns

  • unit8_t


Definition at line 147 of file app/framework/plugin/standalone-bootloader-common/bootloader-protocol.h

sl_zigbee_af_standalone_bootloader_common_send_message#

sl_status_t sl_zigbee_af_standalone_bootloader_common_send_message (bool isBroadcast, sl_802154_long_addr_t targetEui, uint8_t length, uint8_t * message)

Send message.

Parameters
TypeDirectionArgument NameDescription
boolN/AisBroadcast

Ver.: always

sl_802154_long_addr_tN/AtargetEui

Ver.: always

uint8_tN/Alength

Ver.: always

uint8_t *N/Amessage

Ver.: always

Returns

  • sl_status_t status code


Definition at line 159 of file app/framework/plugin/standalone-bootloader-common/bootloader-protocol.h

sl_zigbee_af_standalone_bootloader_common_check_incoming_message#

bool sl_zigbee_af_standalone_bootloader_common_check_incoming_message (uint8_t length, uint8_t * message)

Check incoming message.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Alength

Ver.: always

uint8_t *N/Amessage

Ver.: always

Returns

  • bool true is success


Definition at line 172 of file app/framework/plugin/standalone-bootloader-common/bootloader-protocol.h