WWAH App Event Retry Manager#

API and Callbacks for the WWAH App Event Retry Manager Component.

Silicon Labs proprietary Works With All Hubs (WWAH) app event retry manager.

Modules#

WWAH App Event Retry manager

API#

void

Write attribute-enabled callback.

void

Write attribute queue size callback.

void

WWAH app event retry manager set backoff parameters to default.

API Documentation#

sl_zigbee_af_wwah_app_event_retry_manager_write_attribute_enabled#

void sl_zigbee_af_wwah_app_event_retry_manager_write_attribute_enabled (uint8_t enabled)

Write attribute-enabled callback.

Parameters
N/Aenabled

Ver.: always

This callback is called when the enabled backoff parameter is changed.


Definition at line 63 of file app/framework/plugin/wwah-app-event-retry-manager/wwah-app-event-retry-manager.h

sl_zigbee_af_wwah_app_event_retry_manager_write_attribute_queue_size#

void sl_zigbee_af_wwah_app_event_retry_manager_write_attribute_queue_size (uint8_t queueSize)

Write attribute queue size callback.

Parameters
N/AqueueSize

Ver.: always

This callback is called when the app event retry queue size is being reported.


Definition at line 71 of file app/framework/plugin/wwah-app-event-retry-manager/wwah-app-event-retry-manager.h

sl_zigbee_af_wwah_app_event_retry_manager_set_backoff_params_to_default#

void sl_zigbee_af_wwah_app_event_retry_manager_set_backoff_params_to_default (void )

WWAH app event retry manager set backoff parameters to default.

Parameters
N/A

This callback is called when the app event retry manager is about to set the backoff parameters of the critical message queue provider plugin back to their default.


Definition at line 79 of file app/framework/plugin/wwah-app-event-retry-manager/wwah-app-event-retry-manager.h