sl_bt_evt_gatt_characteristicGATT Client
Indicates that a GATT characteristic in the remote GATT database was discovered.
Data Structures | |
struct | sl_bt_evt_gatt_characteristic_s |
Data structure of the characteristic event. | |
Macros | |
#define | sl_bt_evt_gatt_characteristic_id 0x020900a0 |
Identifier of the characteristic event. | |
Detailed Description
Indicates that a GATT characteristic in the remote GATT database was discovered.
This event is generated after issuing either the sl_bt_gatt_discover_characteristics or sl_bt_gatt_discover_characteristics_by_uuid command.
Data Structure Documentation
◆ sl_bt_evt_gatt_characteristic_s
struct sl_bt_evt_gatt_characteristic_s |
Data structure of the characteristic event.
Data Fields | ||
---|---|---|
uint8_t | connection |
Connection handle |
uint16_t | characteristic |
GATT characteristic handle |
uint8_t | properties |
Characteristic properties |
uint8array | uuid |
Characteristic UUID in little endian format |