Data structure of the friend_remove event.
Public Attribute Documentation#
netkey_index#
uint16_t sl_btmesh_evt_diagnostic_friend_remove_s::netkey_index
Index of the network key used in friendship
Definition at line
22443
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
lpn#
uint16_t sl_btmesh_evt_diagnostic_friend_remove_s::lpn
LPN address
Definition at line
22444
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
src#
uint16_t sl_btmesh_evt_diagnostic_friend_remove_s::src
Source address of the message
Definition at line
22445
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
dst#
uint16_t sl_btmesh_evt_diagnostic_friend_remove_s::dst
Destination address of the message
Definition at line
22446
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
ivi#
uint32_t sl_btmesh_evt_diagnostic_friend_remove_s::ivi
IV index used to secure the message
Definition at line
22447
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
seq#
uint32_t sl_btmesh_evt_diagnostic_friend_remove_s::seq
Sequence number of the message
Definition at line
22448
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
reason#
uint8_t sl_btmesh_evt_diagnostic_friend_remove_s::reason
Reason for removing the message. The following reasons are defined:
0: The message has been acknowledged as delivered by the LPN
1: The message queue has overflowed and the oldest message was dropped
2: A newer segment acknowledgement has been inserted to the message queue
3: Invalidated message segments have been cleaned up
Definition at line
22449
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h