Data structure of the capabilities_status event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_fw_dist_client_capabilities_status_s::elem_index
Client model element index
Definition at line
18389
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
server_address#
uint16_t sl_btmesh_evt_fw_dist_client_capabilities_status_s::server_address
Unicast address of the server
Definition at line
18390
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
max_nodes_list_size#
uint16_t sl_btmesh_evt_fw_dist_client_capabilities_status_s::max_nodes_list_size
Maximum number of entries the node list can contain
Definition at line
18391
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
max_fw_list_size#
uint16_t sl_btmesh_evt_fw_dist_client_capabilities_status_s::max_fw_list_size
Maximum number of entries the Firmware List can contain
Definition at line
18393
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
max_fw_size#
uint32_t sl_btmesh_evt_fw_dist_client_capabilities_status_s::max_fw_size
Maximum size of a single firmware image
Definition at line
18395
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
max_upload_space#
uint32_t sl_btmesh_evt_fw_dist_client_capabilities_status_s::max_upload_space
Maximum number of bytes for firmware images
Definition at line
18397
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
remaining_upload_space#
uint32_t sl_btmesh_evt_fw_dist_client_capabilities_status_s::remaining_upload_space
Remaining number of bytes for firmware images
Definition at line
18399
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
oob_supported#
uint8_t sl_btmesh_evt_fw_dist_client_capabilities_status_s::oob_supported
Enum sl_btmesh_fw_dist_client_dist_oob_t. OOB firmware retrieval (using the Update URI received from an Update Server) supported
Definition at line
18401
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
uri_scheme_names#
uint8array sl_btmesh_evt_fw_dist_client_capabilities_status_s::uri_scheme_names
Supported URI scheme names. Empty if OOB is not supported.
Definition at line
18406
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h