Data structure of the ambient_lux_level_updated event.
Public Attribute Documentation#
destination_address#
uint16_t sl_btmesh_evt_lc_server_ambient_lux_level_updated_s::destination_address
Message destination address
Definition at line
14091
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
elem_index#
uint16_t sl_btmesh_evt_lc_server_ambient_lux_level_updated_s::elem_index
Index of the element where the update happened
Definition at line
14092
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
source_address#
uint16_t sl_btmesh_evt_lc_server_ambient_lux_level_updated_s::source_address
Message source address
Definition at line
14094
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
appkey_index#
uint16_t sl_btmesh_evt_lc_server_ambient_lux_level_updated_s::appkey_index
Message appkey index
Definition at line
14095
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
ambient_lux_level_value#
uint32_t sl_btmesh_evt_lc_server_ambient_lux_level_updated_s::ambient_lux_level_value
The updated value of the LC Ambient LuxLevel state
Definition at line
14096
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h