Data structure of the server_partial_block_report event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_mbt_client_server_partial_block_report_s::elem_index
The client model element index.
Definition at line
10484
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
server_address#
uint16_t sl_btmesh_evt_mbt_client_server_partial_block_report_s::server_address
The MBT Server address.
Definition at line
10485
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
missing_chunks#
uint8array sl_btmesh_evt_mbt_client_server_partial_block_report_s::missing_chunks
A bitfield indicating missing chunks. The least significant bit of the first byte in the array belongs to chunk zero.
Definition at line
10486
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h