Data structure of the config_set event.
Public Attribute Documentation#
netkey_index#
uint16_t sl_btmesh_evt_node_config_set_s::netkey_index
The network key index of the network to which the command applies. 0xffff for node-wide states.
Definition at line
495
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
id#
uint16_t sl_btmesh_evt_node_config_set_s::id
Enum sl_btmesh_node_config_state_t. Specifies to which state the command applies
Definition at line
498
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
value#
uint8array sl_btmesh_evt_node_config_set_s::value
The new value
Definition at line
500
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h