Data structure of the input_oob_request event.
Public Attribute Documentation#
input_action#
uint8_t sl_btmesh_evt_node_input_oob_request_s::input_action
Enum sl_btmesh_node_oob_input_action_t. Selected input action
Definition at line
549
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
input_size#
uint8_t sl_btmesh_evt_node_input_oob_request_s::input_size
Size of data in the input in characters.
Definition at line
551
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h