Data structure of the add_ddb_entry_complete event.

Public Attributes#

uint16_t

Public Attribute Documentation#

result#

uint16_t sl_btmesh_evt_prov_add_ddb_entry_complete_s::result

SL_STATUS_OK if successful. Error code otherwise.


Definition at line 2589 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

uuid#

uuid_128 sl_btmesh_evt_prov_add_ddb_entry_complete_s::uuid

UUID of the Device


Definition at line 2590 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h