OOB Capabilities#
OOB capability bitmask constants
Macros#
#define
#define
#define
#define
#define
#define
#define
#define
#define
SL_BTMESH_PROV_OOB_RFU_8 0x100
#define
SL_BTMESH_PROV_OOB_RFU_9 0x200
#define
SL_BTMESH_PROV_OOB_RFU_A 0x400
#define
#define
#define
SL_BTMESH_PROV_OOB_LOC_PAPER 0x2000
#define
#define
#define
Macro Definition Documentation#
SL_BTMESH_PROV_OOB_OTHER#
#define SL_BTMESH_PROV_OOB_OTHERValue:
0x1
Uncategorized
Definition at line
2150
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_PROV_OOB_URI#
#define SL_BTMESH_PROV_OOB_URIValue:
0x2
URI or other electronic
Definition at line
2153
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_PROV_OOB_2D_MR_CODE#
#define SL_BTMESH_PROV_OOB_2D_MR_CODEValue:
0x4
2D machine-readable code
Definition at line
2156
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_PROV_OOB_BAR_CODE#
#define SL_BTMESH_PROV_OOB_BAR_CODEValue:
0x8
Barcode
Definition at line
2159
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_PROV_OOB_NFC#
#define SL_BTMESH_PROV_OOB_NFCValue:
0x10
NFC
Definition at line
2162
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_PROV_OOB_NUMBER#
#define SL_BTMESH_PROV_OOB_NUMBERValue:
0x20
Number
Definition at line
2165
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_PROV_OOB_STRING#
#define SL_BTMESH_PROV_OOB_STRINGValue:
0x40
String
Definition at line
2168
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_PROV_OOB_RFU_7#
#define SL_BTMESH_PROV_OOB_RFU_7Value:
0x80
Reserved
Definition at line
2171
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_PROV_OOB_RFU_8#
#define SL_BTMESH_PROV_OOB_RFU_8Value:
0x100
Reserved
Definition at line
2174
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_PROV_OOB_RFU_9#
#define SL_BTMESH_PROV_OOB_RFU_9Value:
0x200
Reserved
Definition at line
2177
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_PROV_OOB_RFU_A#
#define SL_BTMESH_PROV_OOB_RFU_AValue:
0x400
Reserved
Definition at line
2180
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_PROV_OOB_LOC_ON_BOX#
#define SL_BTMESH_PROV_OOB_LOC_ON_BOXValue:
0x800
On the box
Definition at line
2183
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_PROV_OOB_LOC_IN_BOX#
#define SL_BTMESH_PROV_OOB_LOC_IN_BOXValue:
0x1000
Inside the box
Definition at line
2186
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_PROV_OOB_LOC_PAPER#
#define SL_BTMESH_PROV_OOB_LOC_PAPERValue:
0x2000
On a piece of paper
Definition at line
2189
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_PROV_OOB_LOC_MANUAL#
#define SL_BTMESH_PROV_OOB_LOC_MANUALValue:
0x4000
In the device manual
Definition at line
2192
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_PROV_OOB_LOC_DEVICE#
#define SL_BTMESH_PROV_OOB_LOC_DEVICEValue:
0x8000
On the device
Definition at line
2195
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
SL_BTMESH_PROV_OOB_RFU_MASK#
#define SL_BTMESH_PROV_OOB_RFU_MASKValue:
0x780
Mask of reserved bits
Definition at line
2198
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h