Data structure of the ddb_list event.

Public Attributes#

uint16_t
uint8_t

Public Attribute Documentation#

uuid#

uuid_128 sl_btmesh_evt_prov_ddb_list_s::uuid

UUID of the Device


Definition at line 2462 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

address#

uint16_t sl_btmesh_evt_prov_ddb_list_s::address

Unicast address of the primary element of the node


Definition at line 2463 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

elements#

uint8_t sl_btmesh_evt_prov_ddb_list_s::elements

Number of elements the device has


Definition at line 2464 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h