Data structure of the delete_ddb_entry_complete event.
Public Attribute Documentation#
result#
uint16_t sl_btmesh_evt_prov_delete_ddb_entry_complete_s::result
SL_STATUS_OK if successful. Error code otherwise.
Definition at line
2613
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
uuid#
uuid_128 sl_btmesh_evt_prov_delete_ddb_entry_complete_s::uuid
UUID of the Device
Definition at line
2614
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h