Data structure of the provisioning_suspended event.

Public Attributes#

uint8_t

Public Attribute Documentation#

uuid#

uuid_128 sl_btmesh_evt_prov_provisioning_suspended_s::uuid

UUID of the device


Definition at line 2240 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

reason#

uint8_t sl_btmesh_evt_prov_provisioning_suspended_s::reason

Reason for suspension. Values are as follows:

  • 0: Capabilities Event received

  • 1: Provisioning link opened


Definition at line 2241 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h