Data structure of the start_sent event.

Public Attribute Documentation#

uuid#

uuid_128 sl_btmesh_evt_prov_start_sent_s::uuid

UUID of the device


Definition at line 2716 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

algorithm#

uint8_t sl_btmesh_evt_prov_start_sent_s::algorithm

Selected provisioning algorithm


Definition at line 2717 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

public_key#

uint8_t sl_btmesh_evt_prov_start_sent_s::public_key

Selected OOB public key


Definition at line 2718 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

authentication_method#

uint8_t sl_btmesh_evt_prov_start_sent_s::authentication_method

Selected authentication method


Definition at line 2719 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

authentication_action#

uint8_t sl_btmesh_evt_prov_start_sent_s::authentication_action

Selected authentication action


Definition at line 2720 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

authentication_size#

uint8_t sl_btmesh_evt_prov_start_sent_s::authentication_size

Selected authentication size


Definition at line 2721 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h