Data structure of the get_request event.
Public Attribute Documentation#
server_address#
uint16_t sl_btmesh_evt_sensor_server_get_request_s::server_address
Destination server address
Definition at line
11655
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
elem_index#
uint16_t sl_btmesh_evt_sensor_server_get_request_s::elem_index
Server model element index
Definition at line
11656
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
client_address#
uint16_t sl_btmesh_evt_sensor_server_get_request_s::client_address
Source client address
Definition at line
11657
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
appkey_index#
uint16_t sl_btmesh_evt_sensor_server_get_request_s::appkey_index
The application key index to use
Definition at line
11658
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
flags#
uint8_t sl_btmesh_evt_sensor_server_get_request_s::flags
No flags defined currently
Definition at line
11659
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
property_id#
uint16_t sl_btmesh_evt_sensor_server_get_request_s::property_id
Property ID for the sensor. Range: 0x0001 - 0x0ffff for a specific device property, or 0x0000 to get the values of all sensors.
Definition at line
11660
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h