Data structure of the server_block_status event.

Public Attributes#

uint16_t
uint8_t

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_mbt_client_server_block_status_s::elem_index

The client model element index.


Definition at line 10474 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

server_address#

uint16_t sl_btmesh_evt_mbt_client_server_block_status_s::server_address

The MBT Server address.


Definition at line 10475 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

status#

uint8_t sl_btmesh_evt_mbt_client_server_block_status_s::status

The status code for the last operation.


Definition at line 10476 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

missing_chunks#

uint8array sl_btmesh_evt_mbt_client_server_block_status_s::missing_chunks

A bitfield indicating missing chunks. The least significant bit of the first byte in the array belongs to chunk zero.


Definition at line 10477 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h