Data structure of the server_failed event.

Public Attributes#

uint16_t
uint8_t
uint8_t

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_mbt_client_server_failed_s::elem_index

The client model element index.


Definition at line 10680 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

server_address#

uint16_t sl_btmesh_evt_mbt_client_server_failed_s::server_address

The MBT Server address.


Definition at line 10681 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

timeout#

uint8_t sl_btmesh_evt_mbt_client_server_failed_s::timeout

Non-zero if a timeout occurred.


Definition at line 10682 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

error#

uint8_t sl_btmesh_evt_mbt_client_server_failed_s::error

Non-zero if an error occurred.


Definition at line 10683 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h