BURTC - Backup RTC
Description
Backup Real Time Counter (BURTC) Peripheral API.
This module contains functions to control the BURTC peripheral of Silicon Labs 32-bit MCUs. The Backup Real Time Counter allows timekeeping in all energy modes. The Backup RTC is also available when the system is in backup mode.
Data Structures |
|
| struct | BURTC_Init_TypeDef |
|
BURTC initialization structure for Series 0 devices.
|
|
Functions |
|
| void | BURTC_IntClear (uint32_t flags) |
|
Clear one or more pending BURTC interrupts.
|
|
| void | BURTC_IntDisable (uint32_t flags) |
|
Disable one or more BURTC interrupts.
|
|
| void | BURTC_IntEnable (uint32_t flags) |
|
Enable one or more BURTC interrupts.
|
|
| uint32_t | BURTC_IntGet (void) |
|
Get pending BURTC interrupt flags.
|
|
| uint32_t | BURTC_IntGetEnabled (void) |
|
Get enabled and pending BURTC interrupt flags.
|
|
| void | BURTC_IntSet (uint32_t flags) |
|
Set one or more pending BURTC interrupts from SW.
|
|
| uint32_t | BURTC_Status (void) |
|
Status of BURTC RAM, timestamp and LP Mode.
|
|
| void | BURTC_StatusClear (void) |
|
Clear and reset BURTC status register.
|
|
| void | BURTC_SyncWait (void) |
|
Wait for the BURTC to complete all synchronization of register changes and commands.
|
|
| uint32_t | BURTC_CounterGet (void) |
|
Get BURTC counter.
|
|
| uint32_t | BURTC_TimestampGet (void) |
|
Get BURTC timestamp for entering BU.
|
|
| void | BURTC_FreezeEnable (bool enable) |
|
Freeze register updates until enabled.
|
|
| void | BURTC_Powerdown (bool enable) |
|
Shut down power to rentention register bank.
|
|
| void | BURTC_RetRegSet (uint32_t num, uint32_t data) |
|
Set a value in one of the retention registers.
|
|
| uint32_t | BURTC_RetRegGet (uint32_t num) |
|
Read a value from one of the retention registers.
|
|
| void | BURTC_Lock (void) |
|
Lock BURTC registers, will protect from writing new config settings.
|
|
| void | BURTC_Unlock (void) |
|
Unlock BURTC registers, enable write access to change configuration.
|
|
| void | BURTC_Reset (void) |
|
Restore BURTC to reset state.
|
|
| void | BURTC_Init (const BURTC_Init_TypeDef *burtcInit) |
|
Initialize BURTC.
|
|
| void | BURTC_Enable (bool enable) |
|
Enable or Disable BURTC peripheral reset and start counter.
|
|
| void | BURTC_CounterReset (void) |
|
Reset counter.
|
|
| void | BURTC_CompareSet (unsigned int comp, uint32_t value) |
|
Set BURTC compare channel.
|
|
| uint32_t | BURTC_CompareGet (unsigned int comp) |
|
Get the BURTC compare value.
|
|
| uint32_t | BURTC_ClockFreqGet (void) |
|
Get the clock frequency of the BURTC.
|
|
Macros |
|
| #define | burtcClkDiv_1 1 |
|
BURTC clock divisors.
|
|
| #define | burtcClkDiv_2 2 |
|
Divide clock by 2.
|
|
| #define | burtcClkDiv_4 4 |
|
Divide clock by 4.
|
|
| #define | burtcClkDiv_8 8 |
|
Divide clock by 8.
|
|
| #define | burtcClkDiv_16 16 |
|
Divide clock by 16.
|
|
| #define | burtcClkDiv_32 32 |
|
Divide clock by 32.
|
|
| #define | burtcClkDiv_64 64 |
|
Divide clock by 64.
|
|
| #define | burtcClkDiv_128 128 |
|
Divide clock by 128.
|
|
| #define | BURTC_INIT_DEFAULT |
|
Default configuration for BURTC initialization structure.
|
|
Enumerations |
|
| enum |
BURTC_ClkSel_TypeDef
{
burtcClkSelULFRCO = BURTC_CTRL_CLKSEL_ULFRCO, burtcClkSelLFRCO = BURTC_CTRL_CLKSEL_LFRCO, burtcClkSelLFXO = BURTC_CTRL_CLKSEL_LFXO } |
|
BURTC clock selection.
|
|
| enum |
BURTC_Mode_TypeDef
{
burtcModeDisable = BURTC_CTRL_MODE_DISABLE, burtcModeEM2 = BURTC_CTRL_MODE_EM2EN, burtcModeEM3 = BURTC_CTRL_MODE_EM3EN, burtcModeEM4 = BURTC_CTRL_MODE_EM4EN } |
|
BURTC mode of operation.
|
|
| enum |
BURTC_LP_TypeDef
{
burtcLPDisable = BURTC_LPMODE_LPMODE_DISABLE, burtcLPEnable = BURTC_LPMODE_LPMODE_ENABLE, burtcLPBU = BURTC_LPMODE_LPMODE_BUEN } |
|
BURTC low power mode.
|
|
Function Documentation
◆ BURTC_IntClear()
|
inline |
Clear one or more pending BURTC interrupts.
- Parameters
-
[in] flagsBURTC interrupt sources to clear. Use a set of interrupt flags OR-ed together to clear multiple interrupt sources for the BURTC module (BURTC_IFS_nnn).
◆ BURTC_IntDisable()
|
inline |
Disable one or more BURTC interrupts.
- Parameters
-
[in] flagsBURTC interrupt sources to disable. Use a set of interrupt flags OR-ed together to disable multiple interrupt sources for the BURTC module (BURTC_IFS_nnn).
◆ BURTC_IntEnable()
|
inline |
Enable one or more BURTC interrupts.
- Note
- Depending on use, a pending interrupt may already be set prior to enabling the interrupt. Consider using BURTC_IntClear() prior to enabling if a pending interrupt should be ignored.
- Parameters
-
[in] flagsBURTC interrupt sources to enable. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for the BURTC module (BURTC_IFS_nnn).
◆ BURTC_IntGet()
|
inline |
Get pending BURTC interrupt flags.
- Note
- This function does not clear the event bits.
- Returns
- Pending BURTC interrupt sources. Returns a set of interrupt flags OR-ed together for multiple interrupt sources in the BURTC module (BURTC_IFS_nnn).
◆ BURTC_IntGetEnabled()
|
inline |
Get enabled and pending BURTC interrupt flags.
- Note
- The event bits are not cleared by the use of this function.
- Returns
- Pending BURTC interrupt sources that is also enabled. Returns a set of interrupt flags OR-ed together for multiple interrupt sources in the BURTC module (BURTC_IFS_nnn).
◆ BURTC_IntSet()
|
inline |
Set one or more pending BURTC interrupts from SW.
- Parameters
-
[in] flagsBURTC interrupt sources to set to pending. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for the BURTC module (BURTC_IFS_nnn).
◆ BURTC_Status()
|
inline |
Status of BURTC RAM, timestamp and LP Mode.
- Returns
- A mask logially OR-ed status bits
◆ BURTC_StatusClear()
|
inline |
Clear and reset BURTC status register.
◆ BURTC_SyncWait()
|
inline |
Wait for the BURTC to complete all synchronization of register changes and commands.
◆ BURTC_CounterGet()
|
inline |
Get BURTC counter.
- Returns
- BURTC counter value
◆ BURTC_TimestampGet()
|
inline |
Get BURTC timestamp for entering BU.
- Returns
- BURTC Time Stamp value
◆ BURTC_FreezeEnable()
|
inline |
Freeze register updates until enabled.
- Parameters
-
[in] enableIf true, registers are not updated until enabled again.
◆ BURTC_Powerdown()
|
inline |
Shut down power to rentention register bank.
- Parameters
-
[in] enableIf true, shuts off power to retention registers.
- Note
- When power rentention is disabled, it cannot be enabled again (until reset).
◆ BURTC_RetRegSet()
|
inline |
Set a value in one of the retention registers.
- Parameters
-
[in] numRegister to set [in] dataValue to put into register
◆ BURTC_RetRegGet()
|
inline |
Read a value from one of the retention registers.
- Parameters
-
[in] numRetention Register to read
- Returns
- Value of the retention register
◆ BURTC_Lock()
|
inline |
Lock BURTC registers, will protect from writing new config settings.
◆ BURTC_Unlock()
|
inline |
Unlock BURTC registers, enable write access to change configuration.
◆ BURTC_Reset()
| void BURTC_Reset | ( | void |
|
) |
Restore BURTC to reset state.
- Note
- Before accessing the BURTC, BURSTEN in RMU->CTRL must be cleared. LOCK will not be reset to default value, as this will disable access to core BURTC registers.
◆ BURTC_Init()
| void BURTC_Init | ( | const BURTC_Init_TypeDef * |
burtcInit
|
) |
Initialize BURTC.
Configures the BURTC peripheral.
- Note
-
Before initialization, BURTC module must first be enabled by clearing the reset bit in the RMU, i.e.,
* RMU_ResetControl(rmuResetBU, rmuResetModeClear); *
Compare channel 0 must be configured outside this function, before initialization if enable is set to true. The counter will always be reset.
- Parameters
-
[in] burtcInitA pointer to the BURTC initialization structure.
◆ BURTC_Enable()
| void BURTC_Enable | ( | bool |
enable
|
) |
Enable or Disable BURTC peripheral reset and start counter.
- Parameters
-
[in] enableIf true; asserts reset to BURTC, halts counter, if false; deassert reset
◆ BURTC_CounterReset()
| void BURTC_CounterReset | ( | void |
|
) |
Reset counter.
◆ BURTC_CompareSet()
| void BURTC_CompareSet | ( | unsigned int |
comp,
|
| uint32_t |
value
|
||
| ) |
Set BURTC compare channel.
- Parameters
-
[in] compCompare the channel index, must be 0 for current devices. [in] valueNew compare value.
◆ BURTC_CompareGet()
| uint32_t BURTC_CompareGet | ( | unsigned int |
comp
|
) |
Get the BURTC compare value.
- Parameters
-
[in] compCompare the channel index value, must be 0 for Giant/Leopard Gecko.
- Returns
- The currently configured value for this compare channel.
◆ BURTC_ClockFreqGet()
| uint32_t BURTC_ClockFreqGet | ( | void |
|
) |
Get the clock frequency of the BURTC.
- Returns
- The current frequency in Hz.
Ultra-low frequency (1 kHz) clock.
Low-frequency RC oscillator.
Low-frequency crystal oscillator.
Macro Definition Documentation
◆ burtcClkDiv_1
| #define burtcClkDiv_1 1 |
BURTC clock divisors.
These values are valid for the BURTC prescaler. Divide clock by 1.
◆ burtcClkDiv_2
| #define burtcClkDiv_2 2 |
Divide clock by 2.
◆ burtcClkDiv_4
| #define burtcClkDiv_4 4 |
Divide clock by 4.
◆ burtcClkDiv_8
| #define burtcClkDiv_8 8 |
Divide clock by 8.
◆ burtcClkDiv_16
| #define burtcClkDiv_16 16 |
Divide clock by 16.
◆ burtcClkDiv_32
| #define burtcClkDiv_32 32 |
Divide clock by 32.
◆ burtcClkDiv_64
| #define burtcClkDiv_64 64 |
Divide clock by 64.
◆ burtcClkDiv_128
| #define burtcClkDiv_128 128 |
Divide clock by 128.
◆ BURTC_INIT_DEFAULT
| #define BURTC_INIT_DEFAULT |
Default configuration for BURTC initialization structure.
Enumeration Type Documentation
◆ BURTC_ClkSel_TypeDef
| enum BURTC_ClkSel_TypeDef |
◆ BURTC_Mode_TypeDef
| enum BURTC_Mode_TypeDef |
◆ BURTC_LP_TypeDef
| enum BURTC_LP_TypeDef |