BURTC_Init_TypeDef Struct Reference
BURTC initialization structure for Series 0 devices.
#include <em_burtc.h>
Data Fields |
|
| bool | enable |
|
Enable BURTC after initialization (starts counter).
|
|
| BURTC_Mode_TypeDef | mode |
|
Configure energy mode operation.
|
|
| bool | debugRun |
|
If true, counter will keep running under debug halt.
|
|
| BURTC_ClkSel_TypeDef | clkSel |
|
Select clock source.
|
|
| uint32_t | clkDiv |
|
Clock divider; for ULFRCO 1Khz or 2kHz operation.
|
|
| uint32_t | lowPowerComp |
|
Number of least significantt clock bits to ignore in low power mode.
|
|
| bool | timeStamp |
|
Enable time stamp on entering backup power domain.
|
|
| bool | compare0Top |
|
Set if Compare Value 0 is also top value (counter restart).
|
|
| BURTC_LP_TypeDef | lowPowerMode |
|
Low power operation mode, requires LFXO or LFRCO.
|
|
BURTC initialization structure for Series 0 devices.
Field Documentation
◆ enable
| bool BURTC_Init_TypeDef::enable |
Enable BURTC after initialization (starts counter).
◆ mode
| BURTC_Mode_TypeDef BURTC_Init_TypeDef::mode |
Configure energy mode operation.
◆ debugRun
| bool BURTC_Init_TypeDef::debugRun |
If true, counter will keep running under debug halt.
◆ clkSel
| BURTC_ClkSel_TypeDef BURTC_Init_TypeDef::clkSel |
Select clock source.
◆ clkDiv
| uint32_t BURTC_Init_TypeDef::clkDiv |
Clock divider; for ULFRCO 1Khz or 2kHz operation.
◆ lowPowerComp
| uint32_t BURTC_Init_TypeDef::lowPowerComp |
Number of least significantt clock bits to ignore in low power mode.
◆ timeStamp
| bool BURTC_Init_TypeDef::timeStamp |
Enable time stamp on entering backup power domain.
◆ compare0Top
| bool BURTC_Init_TypeDef::compare0Top |
Set if Compare Value 0 is also top value (counter restart).
◆ lowPowerMode
| BURTC_LP_TypeDef BURTC_Init_TypeDef::lowPowerMode |
Low power operation mode, requires LFXO or LFRCO.