DMA_Init_TypeDef Struct Reference
DMA initialization structure.
#include <em_dma.h>
Data Fields |
|
| uint8_t | hprot |
|
HPROT signal state when accessing the primary/alternate descriptors.
|
|
| DMA_DESCRIPTOR_TypeDef * | controlBlock |
|
Pointer to the control block in memory holding descriptors (channel control data structures).
|
|
DMA initialization structure.
Field Documentation
◆ hprot
| uint8_t DMA_Init_TypeDef::hprot |
HPROT signal state when accessing the primary/alternate descriptors.
Normally set to 0 if protection is not an issue. The following bits are available:
- bit 0 - HPROT[1] control for descriptor accesses (i.e., when the DMA controller accesses the channel control block itself), privileged/non-privileged access.
◆ controlBlock
| DMA_DESCRIPTOR_TypeDef* DMA_Init_TypeDef::controlBlock |
Pointer to the control block in memory holding descriptors (channel control data structures).
This memory must be properly aligned at a 256 bytes, i.e., the 8 least significant bits must be zero.
Refer to the reference manual, DMA chapter for more details.
It is possible to provide a smaller memory block, only covering those channels actually used, if not all available channels are used. For instance, if only using 4 channels (0-3), both primary and alternate structures, then only 16*2*4 = 128 bytes must be provided. However, this implementation has no check if later exceeding such a limit by configuring for instance channel 4, in which case memory overwrite of some other data will occur.