PCNT_Init_TypeDef Struct Reference
Initialization structure.
#include <em_pcnt.h>
Data Fields |
|
| PCNT_Mode_TypeDef | mode |
|
Mode to operate in.
|
|
| uint32_t | counter |
|
Initial counter value (refer to reference manual for max value allowed).
|
|
| uint32_t | top |
|
Initial top value (refer to reference manual for max value allowed).
|
|
| bool | negEdge |
|
Polarity of incoming edge.
|
|
| bool | countDown |
|
Counting direction, only applicable for
pcntModeOvsSingle
and
pcntModeExtSingle
modes.
|
|
| bool | filter |
|
Enable filter, only available in
pcntModeOvsSingle
* mode.
|
|
| bool | hyst |
|
Set to true to enable hysteresis.
|
|
| bool | s1CntDir |
|
Set to true to enable S1 to determine the direction of counting in OVSSINGLE or EXTCLKSINGLE modes.
|
|
| PCNT_CntEvent_TypeDef | cntEvent |
|
Selects whether the regular counter responds to up-count events, down-count events, both, or none.
|
|
| PCNT_CntEvent_TypeDef | auxCntEvent |
|
Selects whether the auxiliary counter responds to up-count events, down-count events, both, or none.
|
|
| PCNT_PRSSel_TypeDef | s0PRS |
|
Select PRS channel as input to S0IN in PCNTx_INPUT register.
|
|
| PCNT_PRSSel_TypeDef | s1PRS |
|
Select PRS channel as input to S1IN in PCNTx_INPUT register.
|
|
Initialization structure.
Field Documentation
◆ mode
| PCNT_Mode_TypeDef PCNT_Init_TypeDef::mode |
Mode to operate in.
◆ counter
| uint32_t PCNT_Init_TypeDef::counter |
Initial counter value (refer to reference manual for max value allowed).
Only used for pcntModeOvsSingle (and possibly pcntModeDisable ) modes. If using pcntModeExtSingle or pcntModeExtQuad modes, counter value is reset to HW reset value.
◆ top
| uint32_t PCNT_Init_TypeDef::top |
Initial top value (refer to reference manual for max value allowed).
Only used for pcntModeOvsSingle (and possibly pcntModeDisable ) modes. If using pcntModeExtSingle or pcntModeExtQuad modes, top value is reset to HW reset value.
◆ negEdge
| bool PCNT_Init_TypeDef::negEdge |
Polarity of incoming edge.
- pcntModeExtSingle mode - if false, positive edges are counted, otherwise negative edges.
- pcntModeExtQuad mode - if true, counting direction is inverted.
◆ countDown
| bool PCNT_Init_TypeDef::countDown |
Counting direction, only applicable for pcntModeOvsSingle and pcntModeExtSingle modes.
◆ filter
| bool PCNT_Init_TypeDef::filter |
Enable filter, only available in pcntModeOvsSingle * mode.
◆ hyst
| bool PCNT_Init_TypeDef::hyst |
Set to true to enable hysteresis.
When enabled, PCNT will always overflow and underflow to TOP/2.
◆ s1CntDir
| bool PCNT_Init_TypeDef::s1CntDir |
Set to true to enable S1 to determine the direction of counting in OVSSINGLE or EXTCLKSINGLE modes.
When S1 is high, the count direction is given by CNTDIR, and when S1 is low, the count direction is the opposite.
◆ cntEvent
| PCNT_CntEvent_TypeDef PCNT_Init_TypeDef::cntEvent |
Selects whether the regular counter responds to up-count events, down-count events, both, or none.
◆ auxCntEvent
| PCNT_CntEvent_TypeDef PCNT_Init_TypeDef::auxCntEvent |
Selects whether the auxiliary counter responds to up-count events, down-count events, both, or none.
◆ s0PRS
| PCNT_PRSSel_TypeDef PCNT_Init_TypeDef::s0PRS |
Select PRS channel as input to S0IN in PCNTx_INPUT register.
◆ s1PRS
| PCNT_PRSSel_TypeDef PCNT_Init_TypeDef::s1PRS |
Select PRS channel as input to S1IN in PCNTx_INPUT register.