LESENSE_DecStCond_TypeDef Struct Reference
Decoder state condition descriptor structure.
#include <em_lesense.h>
Data Fields |
|
| uint8_t | compVal |
|
Configure compare value.
|
|
| uint8_t | compMask |
|
Configure compare mask.
|
|
| uint8_t | nextState |
|
Configure index of state to be entered if the sensor state equals to compVal.
|
|
| LESENSE_StTransAct_TypeDef | prsAct |
|
Configure which PRS action to perform when the sensor state equals to compVal.
|
|
| bool | setInt |
|
If enabled, interrupt flag is set when sensor state equals to compVal.
|
|
Decoder state condition descriptor structure.
Field Documentation
◆ compVal
| uint8_t LESENSE_DecStCond_TypeDef::compVal |
Configure compare value.
State transition is triggered when the sensor state equals to this value. Valid range: 0-15 (4 bits).
◆ compMask
| uint8_t LESENSE_DecStCond_TypeDef::compMask |
Configure compare mask.
Set bit X to exclude sensor X from evaluation. Note: decoder can handle sensor inputs from up to 4 sensors; therefore, this mask is 4 bit long.
◆ nextState
| uint8_t LESENSE_DecStCond_TypeDef::nextState |
Configure index of state to be entered if the sensor state equals to compVal.
Valid range: 0-15 (4 bits).
◆ prsAct
| LESENSE_StTransAct_TypeDef LESENSE_DecStCond_TypeDef::prsAct |
Configure which PRS action to perform when the sensor state equals to compVal.
◆ setInt
| bool LESENSE_DecStCond_TypeDef::setInt |
If enabled, interrupt flag is set when sensor state equals to compVal.