IADC_SingleInput_t Struct Reference
IADC single input selection structure.
#include <em_iadc.h>
Data Fields | |
IADC_NegInput_t | negInput |
Port/pin input for the negative side of the ADC. | |
IADC_PosInput_t | posInput |
Port/pin input for the positive side of the ADC. | |
uint8_t | configId |
Configuration id. | |
bool | compare |
Perform digital window comparison on the result from this entry. | |
IADC single input selection structure.
Field Documentation
◆ negInput
IADC_NegInput_t IADC_SingleInput_t::negInput |
Port/pin input for the negative side of the ADC.
◆ posInput
IADC_PosInput_t IADC_SingleInput_t::posInput |
Port/pin input for the positive side of the ADC.
◆ configId
uint8_t IADC_SingleInput_t::configId |
Configuration id.
◆ compare
bool IADC_SingleInput_t::compare |
Perform digital window comparison on the result from this entry.