VDAC_InitChannel_TypeDef Struct Reference
VDAC channel initialization structure.
#include <em_vdac.h>
Data Fields | |
bool | enable |
Enable channel. | |
bool | warmupKeepOn |
Warm-up mode, keep VDAC on (in idle) - or shutdown between conversions. | |
bool | highCapLoadEnable |
Select high capacitance load mode in conjunction with high power. | |
uint32_t | fifoLowDataThreshold |
Channel x FIFO Low threshold data valid level. | |
VDAC_RefreshSource_TypeDef | chRefreshSource |
Channel refresh source. | |
VDAC_TrigMode_TypeDef | trigMode |
Channel conversion trigger mode. | |
VDAC_PowerMode_TypeDef | powerMode |
Channel power mode. | |
bool | sampleOffMode |
Set channel conversion mode to sample/shut-off mode. | |
uint32_t | pin |
Vdac channel output pin. | |
VDAC_ChPortSel_t | port |
Vdac channel output port. | |
bool | shortOutput |
Short High power and low power output. | |
bool | auxOutEnable |
Alternative output enable. | |
bool | mainOutEnable |
Main output enable. | |
uint32_t | holdOutTime |
Channel output hold time. | |
VDAC channel initialization structure.
Field Documentation
◆ enable
bool VDAC_InitChannel_TypeDef::enable |
Enable channel.
◆ warmupKeepOn
bool VDAC_InitChannel_TypeDef::warmupKeepOn |
Warm-up mode, keep VDAC on (in idle) - or shutdown between conversions.
◆ highCapLoadEnable
bool VDAC_InitChannel_TypeDef::highCapLoadEnable |
Select high capacitance load mode in conjunction with high power.
◆ fifoLowDataThreshold
uint32_t VDAC_InitChannel_TypeDef::fifoLowDataThreshold |
Channel x FIFO Low threshold data valid level.
◆ chRefreshSource
VDAC_RefreshSource_TypeDef VDAC_InitChannel_TypeDef::chRefreshSource |
Channel refresh source.
◆ trigMode
VDAC_TrigMode_TypeDef VDAC_InitChannel_TypeDef::trigMode |
Channel conversion trigger mode.
◆ powerMode
VDAC_PowerMode_TypeDef VDAC_InitChannel_TypeDef::powerMode |
Channel power mode.
◆ sampleOffMode
bool VDAC_InitChannel_TypeDef::sampleOffMode |
Set channel conversion mode to sample/shut-off mode.
Default is continuous.
◆ pin
uint32_t VDAC_InitChannel_TypeDef::pin |
Vdac channel output pin.
◆ port
VDAC_ChPortSel_t VDAC_InitChannel_TypeDef::port |
Vdac channel output port.
◆ shortOutput
bool VDAC_InitChannel_TypeDef::shortOutput |
Short High power and low power output.
◆ auxOutEnable
bool VDAC_InitChannel_TypeDef::auxOutEnable |
Alternative output enable.
◆ mainOutEnable
bool VDAC_InitChannel_TypeDef::mainOutEnable |
Main output enable.
◆ holdOutTime
uint32_t VDAC_InitChannel_TypeDef::holdOutTime |
Channel output hold time.