IDAC - Current DAC

Description

Current Digital-to-Analog Converter (IDAC) Peripheral API.

IDAC can source or sink a configurable constant current, which can be output on, or sinked from pin or ADC. Current is configurable with several ranges of various step sizes. IDAC can be used with PRS and can operate down to EM3.

The following steps are necessary for basic operation:

Clock enable:

/* IDAC is a HFPERCLK peripheral */

Initialize peripheral with default settings and modify selected fields, such as output select:

/* Initialize with default settings. Change output to APORT1YCH1. */
IDAC_Init(IDAC0, &init);

Set output:

/* Set 50nA step and enable output */
IDAC_StepSet(IDAC0, 0);
IDAC_OutEnable(IDAC0, true);

Data Structures

struct  IDAC_Init_TypeDef
 IDAC initialization structure, common for both channels.
 

Functions

void IDAC_Init (IDAC_TypeDef *idac, const IDAC_Init_TypeDef *init)
 Initialize IDAC.
 
void IDAC_Enable (IDAC_TypeDef *idac, bool enable)
 Enable/disable IDAC.
 
void IDAC_Reset (IDAC_TypeDef *idac)
 Reset IDAC to the same state that it was in after a hardware reset.
 
void IDAC_MinimalOutputTransitionMode (IDAC_TypeDef *idac, bool enable)
 Enable/disable Minimal Output Transition mode.
 
void IDAC_RangeSet (IDAC_TypeDef *idac, const IDAC_Range_TypeDef range)
 Set the current range of the IDAC output.
 
void IDAC_StepSet (IDAC_TypeDef *idac, const uint32_t step)
 Set the current step of the IDAC output.
 
void IDAC_OutEnable (IDAC_TypeDef *idac, bool enable)
 Enable/disable the IDAC OUT pin.
 
void IDAC_OutpadEnable (IDAC_TypeDef *idac, bool enable)
 Enable/disable the IDAC OUTPAD output.
 
void IDAC_IntClear (IDAC_TypeDef *idac, uint32_t flags)
 Clear one or more pending IDAC interrupts.
 
void IDAC_IntDisable (IDAC_TypeDef *idac, uint32_t flags)
 Disable one or more IDAC interrupts.
 
void IDAC_IntEnable (IDAC_TypeDef *idac, uint32_t flags)
 Enable one or more IDAC interrupts.
 
uint32_t IDAC_IntGet (IDAC_TypeDef *idac)
 Get pending IDAC interrupt flags.
 
uint32_t IDAC_IntGetEnabled (IDAC_TypeDef *idac)
 Get enabled and pending IDAC interrupt flags.
 
void IDAC_IntSet (IDAC_TypeDef *idac, uint32_t flags)
 Set one or more pending IDAC interrupts from SW.
 

Macros

#define IDAC_INIT_DEFAULT
 Default configuration for IDAC initialization structure.
 

Enumerations

enum  IDAC_OutMode_TypeDef {
  idacOutputAPORT1XCH0 = IDAC_CTRL_APORTOUTSEL_APORT1XCH0,
  idacOutputAPORT1YCH1 = IDAC_CTRL_APORTOUTSEL_APORT1YCH1,
  idacOutputAPORT1XCH2 = IDAC_CTRL_APORTOUTSEL_APORT1XCH2,
  idacOutputAPORT1YCH3 = IDAC_CTRL_APORTOUTSEL_APORT1YCH3,
  idacOutputAPORT1XCH4 = IDAC_CTRL_APORTOUTSEL_APORT1XCH4,
  idacOutputAPORT1YCH5 = IDAC_CTRL_APORTOUTSEL_APORT1YCH5,
  idacOutputAPORT1XCH6 = IDAC_CTRL_APORTOUTSEL_APORT1XCH6,
  idacOutputAPORT1YCH7 = IDAC_CTRL_APORTOUTSEL_APORT1YCH7,
  idacOutputAPORT1XCH8 = IDAC_CTRL_APORTOUTSEL_APORT1XCH8,
  idacOutputAPORT1YCH9 = IDAC_CTRL_APORTOUTSEL_APORT1YCH9,
  idacOutputAPORT1XCH10 = IDAC_CTRL_APORTOUTSEL_APORT1XCH10,
  idacOutputAPORT1YCH11 = IDAC_CTRL_APORTOUTSEL_APORT1YCH11,
  idacOutputAPORT1XCH12 = IDAC_CTRL_APORTOUTSEL_APORT1XCH12,
  idacOutputAPORT1YCH13 = IDAC_CTRL_APORTOUTSEL_APORT1YCH13,
  idacOutputAPORT1XCH14 = IDAC_CTRL_APORTOUTSEL_APORT1XCH14,
  idacOutputAPORT1YCH15 = IDAC_CTRL_APORTOUTSEL_APORT1YCH15,
  idacOutputAPORT1XCH16 = IDAC_CTRL_APORTOUTSEL_APORT1XCH16,
  idacOutputAPORT1YCH17 = IDAC_CTRL_APORTOUTSEL_APORT1YCH17,
  idacOutputAPORT1XCH18 = IDAC_CTRL_APORTOUTSEL_APORT1XCH18,
  idacOutputAPORT1YCH19 = IDAC_CTRL_APORTOUTSEL_APORT1YCH19,
  idacOutputAPORT1XCH20 = IDAC_CTRL_APORTOUTSEL_APORT1XCH20,
  idacOutputAPORT1YCH21 = IDAC_CTRL_APORTOUTSEL_APORT1YCH21,
  idacOutputAPORT1XCH22 = IDAC_CTRL_APORTOUTSEL_APORT1XCH22,
  idacOutputAPORT1YCH23 = IDAC_CTRL_APORTOUTSEL_APORT1YCH23,
  idacOutputAPORT1XCH24 = IDAC_CTRL_APORTOUTSEL_APORT1XCH24,
  idacOutputAPORT1YCH25 = IDAC_CTRL_APORTOUTSEL_APORT1YCH25,
  idacOutputAPORT1XCH26 = IDAC_CTRL_APORTOUTSEL_APORT1XCH26,
  idacOutputAPORT1YCH27 = IDAC_CTRL_APORTOUTSEL_APORT1YCH27,
  idacOutputAPORT1XCH28 = IDAC_CTRL_APORTOUTSEL_APORT1XCH28,
  idacOutputAPORT1YCH29 = IDAC_CTRL_APORTOUTSEL_APORT1YCH29,
  idacOutputAPORT1XCH30 = IDAC_CTRL_APORTOUTSEL_APORT1XCH30,
  idacOutputAPORT1YCH31 = IDAC_CTRL_APORTOUTSEL_APORT1YCH31
}
 Output mode.
 
enum  IDAC_PRSSEL_TypeDef {
  idacPRSSELCh0 = IDAC_CTRL_PRSSEL_PRSCH0,
  idacPRSSELCh1 = IDAC_CTRL_PRSSEL_PRSCH1,
  idacPRSSELCh2 = IDAC_CTRL_PRSSEL_PRSCH2,
  idacPRSSELCh3 = IDAC_CTRL_PRSSEL_PRSCH3,
  idacPRSSELCh4 = IDAC_CTRL_PRSSEL_PRSCH4,
  idacPRSSELCh5 = IDAC_CTRL_PRSSEL_PRSCH5,
  idacPRSSELCh6 = IDAC_CTRL_PRSSEL_PRSCH6,
  idacPRSSELCh7 = IDAC_CTRL_PRSSEL_PRSCH7,
  idacPRSSELCh8 = IDAC_CTRL_PRSSEL_PRSCH8,
  idacPRSSELCh9 = IDAC_CTRL_PRSSEL_PRSCH9,
  idacPRSSELCh10 = IDAC_CTRL_PRSSEL_PRSCH10,
  idacPRSSELCh11 = IDAC_CTRL_PRSSEL_PRSCH11
}
 Selects which Peripheral Reflex System (PRS) signal to use when PRS is set to control IDAC output.
 
enum  IDAC_Range_TypeDef {
  idacCurrentRange0 = IDAC_CURPROG_RANGESEL_RANGE0,
  idacCurrentRange1 = IDAC_CURPROG_RANGESEL_RANGE1,
  idacCurrentRange2 = IDAC_CURPROG_RANGESEL_RANGE2,
  idacCurrentRange3 = IDAC_CURPROG_RANGESEL_RANGE3
}
 Selects which current range to use.
 

Function Documentation

◆ IDAC_Init()

void IDAC_Init ( IDAC_TypeDef *  idac,
const IDAC_Init_TypeDef init 
)

Initialize IDAC.

Initializes IDAC according to the initialization structure parameter and sets the default calibration value stored in the DEVINFO structure.

Note
This function will disable IDAC prior to configuration.
Parameters
[in]idacA pointer to the IDAC peripheral register block.
[in]initA pointer to the IDAC initialization structure.

◆ IDAC_Enable()

void IDAC_Enable ( IDAC_TypeDef *  idac,
bool  enable 
)

Enable/disable IDAC.

Parameters
[in]idacA pointer to the IDAC peripheral register block.
[in]enableTrue to enable IDAC, false to disable.

◆ IDAC_Reset()

void IDAC_Reset ( IDAC_TypeDef *  idac)

Reset IDAC to the same state that it was in after a hardware reset.

Parameters
[in]idacA pointer to the IDAC peripheral register block.

◆ IDAC_MinimalOutputTransitionMode()

void IDAC_MinimalOutputTransitionMode ( IDAC_TypeDef *  idac,
bool  enable 
)

Enable/disable Minimal Output Transition mode.

Parameters
[in]idacA pointer to the IDAC peripheral register block.
[in]enableTrue to enable Minimal Output Transition mode, false to disable.

◆ IDAC_RangeSet()

void IDAC_RangeSet ( IDAC_TypeDef *  idac,
const IDAC_Range_TypeDef  range 
)

Set the current range of the IDAC output.

This function sets the current range of the IDAC output. The function also updates the IDAC calibration register (IDAC_CAL) with the default calibration value from DEVINFO (factory calibration) corresponding to the specified range.

Parameters
[in]idacA pointer to the IDAC peripheral register block.
[in]rangeThe current range value.

◆ IDAC_StepSet()

void IDAC_StepSet ( IDAC_TypeDef *  idac,
const uint32_t  step 
)

Set the current step of the IDAC output.

Parameters
[in]idacA pointer to the IDAC peripheral register block.
[in]stepA step value for the IDAC output. A valid range is 0-31.

◆ IDAC_OutEnable()

void IDAC_OutEnable ( IDAC_TypeDef *  idac,
bool  enable 
)

Enable/disable the IDAC OUT pin.

Warning
This function will not enable/disable the IDAC OUT pin if APORTOUTENPRS is set because output enable will be controlled by PRS.
Parameters
[in]idacA pointer to the IDAC peripheral register block.
[in]enableTrue to enable the IDAC OUT pin, false to disable.

◆ IDAC_OutpadEnable()

void IDAC_OutpadEnable ( IDAC_TypeDef *  idac,
bool  enable 
)

Enable/disable the IDAC OUTPAD output.

Note
IDAC OUTPAD is not available on some EFR32xG1 series devices as well as on non-BGA125 EFR32MG12 devices either because of lack of that feature (former) or because OUTPAD pin is not available on other packages (latter).
Warning
This function will not enable/disable the IDAC OUTPAD pin if MAINOUTENPRS is set because output enable will be controlled by PRS.
Parameters
[in]idacA pointer to the IDAC peripheral register block.
[in]enableTrue to enable the IDAC OUTPAD, false to disable.

◆ IDAC_IntClear()

void IDAC_IntClear ( IDAC_TypeDef *  idac,
uint32_t  flags 
)
inline

Clear one or more pending IDAC interrupts.

Parameters
[in]idacPointer to IDAC peripheral register block.
[in]flagsPending IDAC interrupt source(s) to clear. Use one or more valid interrupt flags for the IDAC module (IDAC_IF_nnn) OR'ed together.

◆ IDAC_IntDisable()

void IDAC_IntDisable ( IDAC_TypeDef *  idac,
uint32_t  flags 
)
inline

Disable one or more IDAC interrupts.

Parameters
[in]idacPointer to IDAC peripheral register block.
[in]flagsIDAC interrupt source(s) to disable. Use one or more valid interrupt flags for the IDAC module (IDAC_IF_nnn) OR'ed together.

◆ IDAC_IntEnable()

void IDAC_IntEnable ( IDAC_TypeDef *  idac,
uint32_t  flags 
)
inline

Enable one or more IDAC interrupts.

Note
Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using IDAC_IntClear() prior to enabling the interrupt.
Parameters
[in]idacPointer to IDAC peripheral register block.
[in]flagsIDAC interrupt source(s) to enable. Use one or more valid interrupt flags for IDAC module (IDAC_IF_nnn) OR'ed together.

◆ IDAC_IntGet()

uint32_t IDAC_IntGet ( IDAC_TypeDef *  idac)
inline

Get pending IDAC interrupt flags.

Note
Event bits are not cleared by the use of this function.
Parameters
[in]idacPointer to IDAC peripheral register block.
Returns
IDAC interrupt source(s) pending. Returns one or more valid interrupt flags for IDAC module (IDAC_IF_nnn) OR'ed together.

◆ IDAC_IntGetEnabled()

uint32_t IDAC_IntGetEnabled ( IDAC_TypeDef *  idac)
inline

Get enabled and pending IDAC interrupt flags.

Useful for handling more interrupt sources in the same interrupt handler.

Parameters
[in]idacPointer to IDAC peripheral register block.
Note
Interrupt flags are not cleared by the use of this function.
Returns
Pending and enabled IDAC interrupt sources. Return value is the bitwise AND combination of
  • the OR combination of enabled interrupt sources in IDACx_IEN_nnn register (IDACx_IEN_nnn) and
  • the OR combination of valid interrupt flags of IDAC module (IDACx_IF_nnn).

◆ IDAC_IntSet()

void IDAC_IntSet ( IDAC_TypeDef *  idac,
uint32_t  flags 
)
inline

Set one or more pending IDAC interrupts from SW.

Parameters
[in]idacPointer to IDAC peripheral register block.
[in]flagsIDAC interrupt source(s) to set to pending. Use one or more valid interrupt flags for IDAC module (IDAC_IF_nnn) OR'ed together.

Macro Definition Documentation

◆ IDAC_INIT_DEFAULT

#define IDAC_INIT_DEFAULT
Value:
{ \
false, \
idacOutputAPORT1XCH0, \
false, \
false, \
idacPRSSELCh0, \
false \
}

Default configuration for IDAC initialization structure.

Enumeration Type Documentation

◆ IDAC_OutMode_TypeDef

Output mode.

Enumerator
idacOutputAPORT1XCH0 

Output to APORT 1X CH0.

idacOutputAPORT1YCH1 

Output to APORT 1Y CH1.

idacOutputAPORT1XCH2 

Output to APORT 1X CH2.

idacOutputAPORT1YCH3 

Output to APORT 1Y CH3.

idacOutputAPORT1XCH4 

Output to APORT 1X CH4.

idacOutputAPORT1YCH5 

Output to APORT 1Y CH5.

idacOutputAPORT1XCH6 

Output to APORT 1X CH6.

idacOutputAPORT1YCH7 

Output to APORT 1Y CH7.

idacOutputAPORT1XCH8 

Output to APORT 1X CH8.

idacOutputAPORT1YCH9 

Output to APORT 1Y CH9.

idacOutputAPORT1XCH10 

Output to APORT 1X CH10.

idacOutputAPORT1YCH11 

Output to APORT 1Y CH11.

idacOutputAPORT1XCH12 

Output to APORT 1X CH12.

idacOutputAPORT1YCH13 

Output to APORT 1Y CH13.

idacOutputAPORT1XCH14 

Output to APORT 1X CH14.

idacOutputAPORT1YCH15 

Output to APORT 1Y CH15.

idacOutputAPORT1XCH16 

Output to APORT 1X CH16.

idacOutputAPORT1YCH17 

Output to APORT 1Y CH17.

idacOutputAPORT1XCH18 

Output to APORT 1X CH18.

idacOutputAPORT1YCH19 

Output to APORT 1Y CH19.

idacOutputAPORT1XCH20 

Output to APORT 1X CH20.

idacOutputAPORT1YCH21 

Output to APORT 1Y CH21.

idacOutputAPORT1XCH22 

Output to APORT 1X CH22.

idacOutputAPORT1YCH23 

Output to APORT 1Y CH23.

idacOutputAPORT1XCH24 

Output to APORT 1X CH24.

idacOutputAPORT1YCH25 

Output to APORT 1Y CH25.

idacOutputAPORT1XCH26 

Output to APORT 1X CH26.

idacOutputAPORT1YCH27 

Output to APORT 1Y CH27.

idacOutputAPORT1XCH28 

Output to APORT 1X CH28.

idacOutputAPORT1YCH29 

Output to APORT 1Y CH29.

idacOutputAPORT1XCH30 

Output to APORT 1X CH30.

idacOutputAPORT1YCH31 

Output to APORT 1Y CH31.

◆ IDAC_PRSSEL_TypeDef

Selects which Peripheral Reflex System (PRS) signal to use when PRS is set to control IDAC output.

Enumerator
idacPRSSELCh0 

PRS channel 0.

idacPRSSELCh1 

PRS channel 1.

idacPRSSELCh2 

PRS channel 2.

idacPRSSELCh3 

PRS channel 3.

idacPRSSELCh4 

PRS channel 4.

idacPRSSELCh5 

PRS channel 5.

idacPRSSELCh6 

PRS channel 6.

idacPRSSELCh7 

PRS channel 7.

idacPRSSELCh8 

PRS channel 8.

idacPRSSELCh9 

PRS channel 9.

idacPRSSELCh10 

PRS channel 10.

idacPRSSELCh11 

PRS channel 11.

◆ IDAC_Range_TypeDef

Selects which current range to use.

Enumerator
idacCurrentRange0 

current range 0.

idacCurrentRange1 

current range 1.

idacCurrentRange2 

current range 2.

idacCurrentRange3 

current range 3.