EMU - Energy Management Unit
Description
Energy Management Unit (EMU) Peripheral API.
This module contains functions to control the EMU peripheral of Silicon Labs 32-bit MCUs and SoCs. The EMU handles the different low energy modes in Silicon Labs microcontrollers.
| Data Structures | |
| struct | EMU_EM01Init_TypeDef | 
| EM0 and 1 initialization structure. | |
| struct | EMU_EM23Init_TypeDef | 
| EM2 and 3 initialization structure. | |
| struct | EMU_EM4Init_TypeDef | 
| EM4 initialization structure. | |
| Functions | |
| void | EMU_EM01Init (const EMU_EM01Init_TypeDef *em01Init) | 
| Update the EMU module with Energy Mode 0 and 1 configuration. | |
| void | EMU_EM23Init (const EMU_EM23Init_TypeDef *em23Init) | 
| Update the EMU module with Energy Mode 2 and 3 configuration. | |
| void | EMU_EM23PresleepHook (void) | 
| Energy mode 2/3 pre-sleep hook function. | |
| void | EMU_EFPEM23PresleepHook (void) | 
| EFP's Energy mode 2/3 pre-sleep hook function. | |
| void | EMU_EM23PostsleepHook (void) | 
| Energy mode 2/3 post-sleep hook function. | |
| void | EMU_EFPEM23PostsleepHook (void) | 
| EFP's Energy mode 2/3 post-sleep hook function. | |
| void | EMU_EnterEM2 (bool restore) | 
| Enter energy mode 2 (EM2). | |
| void | EMU_EnterEM3 (bool restore) | 
| Enter energy mode 3 (EM3). | |
| void | EMU_Save (void) | 
| Save the CMU HF clock select state, oscillator enable, and voltage scaling (if available) before
         
          EMU_EnterEM2()
         
         or
         
          EMU_EnterEM3()
         
         are called with the restore parameter set to false. | |
| void | EMU_Restore (void) | 
| Restore CMU HF clock select state, oscillator enable, and voltage scaling (if available) after
         
          EMU_EnterEM2()
         
         or
         
          EMU_EnterEM3()
         
         are called with the restore parameter set to false. | |
| void | EMU_EM4Init (const EMU_EM4Init_TypeDef *em4Init) | 
| Update the EMU module with Energy Mode 4 configuration. | |
| void | EMU_EM4PresleepHook (void) | 
| Energy mode 4 pre-sleep hook function. | |
| void | EMU_EFPEM4PresleepHook (void) | 
| EFP's Energy mode 4 pre-sleep hook function. | |
| void | EMU_EnterEM4 (void) | 
| Enter energy mode 4 (EM4). | |
| void | EMU_EnterEM4H (void) | 
| Enter energy mode 4 hibernate (EM4H). | |
| void | EMU_EnterEM4S (void) | 
| Enter energy mode 4 shutoff (EM4S). | |
| void | EMU_MemPwrDown (uint32_t blocks) | 
| Power down memory block. | |
| void | EMU_RamPowerDown (uint32_t start, uint32_t end) | 
| Power down RAM memory blocks. | |
| void | EMU_RamPowerUp (void) | 
| Power up all available RAM memory blocks. | |
| void | EMU_UpdateOscConfig (void) | 
| Update EMU module with CMU oscillator selection/enable status. | |
| void | EMU_EFPEM01VScale ( EMU_VScaleEM01_TypeDef voltage) | 
| Energy mode 01 voltage scaling hook function. | |
| void | EMU_VScaleEM01ByClock (uint32_t clockFrequency, bool wait) | 
| Voltage scale in EM0 and 1 by clock frequency. | |
| void | EMU_VScaleEM01 ( EMU_VScaleEM01_TypeDef voltage, bool wait) | 
| Force voltage scaling in EM0 and 1 to a specific voltage level. | |
| float | EMU_TemperatureGet (void) | 
| Get temperature in degrees Celsius. | |
| void | EMU_EFPDirectModeEnable (bool enable) | 
| Enable/disable EFP Direct Mode. | |
| void | EMU_EFPDriveDecoupleSet (bool enable) | 
| Set to enable EFP to drive Decouple voltage. | |
| void | EMU_EFPDriveDvddSet (bool enable) | 
| Set to enable EFP to drive DVDD voltage. | |
| void | EMU_DCDCLock (void) | 
| Lock DCDC registers in order to protect them against unintended modification. | |
| void | EMU_DCDCUnlock (void) | 
| Unlock the DCDC so that writing to locked registers again is possible. | |
| void | EMU_DCDCSync (uint32_t mask) | 
| Wait for the DCDC to complete all synchronization of register changes. | |
| void | EMU_EnterEM1 (void) | 
| Enter energy mode 1 (EM1). | |
| void | EMU_VScaleWait (void) | 
| Wait for voltage scaling to complete. | |
| EMU_VScaleEM01_TypeDef | EMU_VScaleGet (void) | 
| Get current voltage scaling level. | |
| void | EMU_IntClear (uint32_t flags) | 
| Clear one or more pending EMU interrupts. | |
| void | EMU_IntDisable (uint32_t flags) | 
| Disable one or more EMU interrupts. | |
| void | EMU_IntEnable (uint32_t flags) | 
| Enable one or more EMU interrupts. | |
| void | EMU_EFPIntEnable (uint32_t flags) | 
| Enable EFP interrupts. | |
| uint32_t | EMU_EFPIntGet (void) | 
| Get pending EMU EFP interrupt flags. | |
| void | EMU_EFPIntClear (uint32_t flags) | 
| Clear one or more pending EMU EFP interrupts. | |
| uint32_t | EMU_IntGet (void) | 
| Get pending EMU interrupt flags. | |
| uint32_t | EMU_IntGetEnabled (void) | 
| Get enabled and pending EMU interrupt flags. | |
| void | EMU_IntSet (uint32_t flags) | 
| Set one or more pending EMU interrupts. | |
| void | EMU_Lock (void) | 
| Lock EMU registers in order to protect them against unintended modification. | |
| void | EMU_Unlock (void) | 
| Unlock the EMU so that writing to locked registers again is possible. | |
| void | EMU_UnlatchPinRetention (void) | 
| When EM4 pin retention is set to emuPinRetentionLatch, then pins are retained through EM4 entry and wakeup. | |
| bool | EMU_TemperatureReady (void) | 
| Temperature measurement ready status. | |
| float | EMU_TemperatureAvgGet (void) | 
| Get averaged temperature in degrees Celsius. | |
| void | EMU_TemperatureAvgRequest ( EMU_TempAvgNum_TypeDef numSamples) | 
| Request averaged temperature. | |
| Macros | |
| #define | EMU_VSCALE_PRESENT | 
| Voltage scaling present. | |
| #define | EMU_VSCALE_EM01_PRESENT | 
| Voltage scaling for EM01 present. | |
| #define | EMU_EM01INIT_DEFAULT | 
| Default initialization of EM0 and 1 configuration. | |
| #define | EMU_EM23INIT_DEFAULT | 
| Default initialization of EM2 and 3 configuration. | |
| #define | EMU_EM4INIT_DEFAULT | 
| Default initialization of EM4 configuration (Series 1 without VSCALE). | |
| #define | EMU_TEMP_ZERO_C_IN_KELVIN (273.15f) | 
| Zero degrees Celcius in Kelvin. | |
| Enumerations | |
| enum | EMU_BODMode_TypeDef
         
         { emuBODMode_Active , emuBODMode_Inactive } | 
| BOD threshold setting selector, active or inactive mode. | |
| enum | EMU_EM4State_TypeDef
         
         { emuEM4Shutoff = 0, emuEM4Hibernate = 1 } | 
| EM4 modes. | |
| enum | EMU_EM4PinRetention_TypeDef
         
         { emuPinRetentionDisable = EMU_EM4CTRL_EM4IORETMODE_DISABLE, emuPinRetentionEm4Exit = EMU_EM4CTRL_EM4IORETMODE_EM4EXIT, emuPinRetentionLatch = EMU_EM4CTRL_EM4IORETMODE_SWUNLATCH } | 
| EM4 Pin Retention Type. | |
| enum | EMU_PowerConfig_TypeDef { emuPowerConfig_DcdcToDvdd } | 
| Power configurations. | |
| enum | EMU_VScaleEM01_TypeDef
         
         { emuVScaleEM01_HighPerformance = _EMU_STATUS_VSCALE_VSCALE2, emuVScaleEM01_LowPower = _EMU_STATUS_VSCALE_VSCALE1 } | 
| Supported EM0/1 Voltage Scaling Levels. | |
| enum | EMU_VScaleEM23_TypeDef
         
         { emuVScaleEM23_FastWakeup = _EMU_CTRL_EM23VSCALE_VSCALE2, emuVScaleEM23_LowPower = _EMU_CTRL_EM23VSCALE_VSCALE0 } | 
| Supported EM2/3 Voltage Scaling Levels. | |
| enum | EMU_TempAvgNum_TypeDef
         
         { emuTempAvgNum_16 = _EMU_CTRL_TEMPAVGNUM_N16, emuTempAvgNum_64 = _EMU_CTRL_TEMPAVGNUM_N64 } | 
| Number of samples to use for temperature averaging. | |
Function Documentation
◆ EMU_EM01Init()
| void EMU_EM01Init | ( | const EMU_EM01Init_TypeDef * | 
            em01Init
            | ) | 
Update the EMU module with Energy Mode 0 and 1 configuration.
- Parameters
- 
         [in] em01InitEnergy Mode 0 and 1 configuration structure. 
◆ EMU_EM23Init()
| void EMU_EM23Init | ( | const EMU_EM23Init_TypeDef * | 
            em23Init
            | ) | 
Update the EMU module with Energy Mode 2 and 3 configuration.
- Parameters
- 
         [in] em23InitEnergy Mode 2 and 3 configuration structure. 
◆ EMU_EM23PresleepHook()
| void EMU_EM23PresleepHook | ( | void | 
            | ) | 
Energy mode 2/3 pre-sleep hook function.
This function is called by EMU_EnterEM2() and EMU_EnterEM3() functions just prior to execution of the WFI instruction. The function implementation does not perform anything, but it is SL_WEAK so that it can be re- implemented in application code if actions are needed.
◆ EMU_EFPEM23PresleepHook()
| void EMU_EFPEM23PresleepHook | ( | void | 
            | ) | 
EFP's Energy mode 2/3 pre-sleep hook function.
This function is similar to EMU_EM23PresleepHook() but is reserved for EFP usage.
- Note
- The function is primarily meant to be used in systems with EFP circuitry. (EFP = Energy Friendly Pmic (PMIC = Power Management IC)). In such systems there is a need to drive certain signals to EFP pins to notify about energy mode transitions.
◆ EMU_EM23PostsleepHook()
| void EMU_EM23PostsleepHook | ( | void | 
            | ) | 
Energy mode 2/3 post-sleep hook function.
This function is called by EMU_EnterEM2() and EMU_EnterEM3() functions just after wakeup from the WFI instruction. The function implementation does not perform anything, but it is SL_WEAK so that it can be re- implemented in application code if actions are needed.
◆ EMU_EFPEM23PostsleepHook()
| void EMU_EFPEM23PostsleepHook | ( | void | 
            | ) | 
EFP's Energy mode 2/3 post-sleep hook function.
This function is similar to EMU_EM23PostsleepHook() but is reserved for EFP usage.
- Note
- The function is primarily meant to be used in systems with EFP circuitry. (EFP = Energy Friendly Pmic (PMIC = Power Management IC)). In such systems there is a need to drive certain signals to EFP pins to notify about energy mode transitions.
◆ EMU_EnterEM2()
| void EMU_EnterEM2 | ( | bool | 
            restore
            | ) | 
Enter energy mode 2 (EM2).
When entering EM2, high-frequency clocks are disabled, i.e., HFXO, HFRCO and AUXHFRCO (for AUXHFRCO, see exception note below). When re-entering EM0, HFRCO is re-enabled and the core will be clocked by the configured HFRCO band. This ensures a quick wakeup from EM2.
        However, prior to entering EM2, the core may have been using another oscillator than HFRCO. The
        
         restore
        
        parameter gives the user the option to restore all HF oscillators according to state prior to entering EM2, as well as the clock used to clock the core. This restore procedure is handled by SW. However, since handled by SW, it will not be restored before completing the interrupt function(s) waking up the core!
       
- Note
- If restoring core clock to use the HFXO oscillator, which has been disabled during EM2 mode, this function will stall until the oscillator has stabilized. Stalling time can be reduced by adding interrupt support detecting stable oscillator, and an asynchronous switch to the original oscillator. See CMU documentation. Such a feature is however outside the scope of the implementation in this function.
- If ERRATA_FIX_EMU_E110_ENABLE is active, the core's SLEEPONEXIT feature can not be used.
- If HFXO is re-enabled by this function, and NOT used to clock the core, this function will not wait for HFXO to stabilize. This must be considered by the application if trying to use features relying on that oscillator upon return.
- 
         If a debugger is attached, the AUXHFRCO will not be disabled if enabled upon entering EM2. It will thus remain enabled when returning to EM0 regardless of the
         restoreparameter.
- 
         If HFXO autostart and select is enabled by using CMU_HFXOAutostartEnable(), the automatic starting and selecting of the core clocks will be done, regardless of the
         restoreparameter, when waking up on the wakeup sources corresponding to the autostart and select setting.
- If voltage scaling is supported, the restore parameter is true and the EM0 voltage scaling level is set higher than the EM2 level, then the EM0 level is also restored.
- 
         On Series 2 Config 2 devices (EFRxG22), this function will also relock the DPLL if the DPLL is used and
         restoreis true.
Note that the hardware will automatically update the HFRCO frequency in the case where voltage scaling is used in EM2/EM3 and not in EM0/EM1. When the restore argument to this function is true then software will restore the original HFRCO frequency after EM2/EM3 wake up. If the restore argument is false then the HFRCO frequency is 19 MHz when coming out of EM2/EM3 and all wait states are at a safe value.
- Parameters
- 
         [in] restore- true - save and restore oscillators, clocks and voltage scaling, see function details.
- false - do not save and restore oscillators and clocks, see function details.
 
- 
         The
         restoreoption should only be used if all clock control is done via the CMU API.
◆ EMU_EnterEM3()
| void EMU_EnterEM3 | ( | bool | 
            restore
            | ) | 
Enter energy mode 3 (EM3).
When entering EM3, the high-frequency clocks are disabled by hardware, i.e., HFXO, HFRCO, and AUXHFRCO (for AUXHFRCO, see exception note below). In addition, the low-frequency clocks, i.e., LFXO and LFRCO are disabled by software. When re-entering EM0, HFRCO is re-enabled and the core will be clocked by the configured HFRCO band. This ensures a quick wakeup from EM3.
        However, prior to entering EM3, the core may have been using an oscillator other than HFRCO. The
        
         restore
        
        parameter gives the user the option to restore all HF/LF oscillators according to state prior to entering EM3, as well as the clock used to clock the core. This restore procedure is handled by software. However, since it is handled by software, it will not be restored before completing the interrupt function(s) waking up the core!
       
- Note
- If restoring core clock to use an oscillator other than HFRCO, this function will stall until the oscillator has stabilized. Stalling time can be reduced by adding interrupt support detecting stable oscillator, and an asynchronous switch to the original oscillator. See CMU documentation. This feature is, however, outside the scope of the implementation in this function.
- If ERRATA_FIX_EMU_E110_ENABLE is active, the core's SLEEPONEXIT feature can't be used.
- If HFXO/LFXO/LFRCO are re-enabled by this function, and NOT used to clock the core, this function will not wait for those oscillators to stabilize. This must be considered by the application if trying to use features relying on those oscillators upon return.
- 
         If a debugger is attached, the AUXHFRCO will not be disabled if enabled upon entering EM3. It will, therefore, remain enabled when returning to EM0 regardless of the
         restoreparameter.
- If voltage scaling is supported, the restore parameter is true and the EM0 voltage scaling level is set higher than the EM3 level, then the EM0 level is also restored.
- 
         On Series 2 Config 2 devices (EFRxG22), this function will also relock the DPLL if the DPLL is used and
         restoreis true.
- Parameters
- 
         [in] restore- true - save and restore oscillators, clocks and voltage scaling, see function details.
- false - do not save and restore oscillators and clocks, see function details.
 
- 
         The
         restoreoption should only be used if all clock control is done via the CMU API.
◆ EMU_Save()
| void EMU_Save | ( | void | 
            | ) | 
Save the CMU HF clock select state, oscillator enable, and voltage scaling (if available) before EMU_EnterEM2() or EMU_EnterEM3() are called with the restore parameter set to false.
Calling this function is equivalent to calling EMU_EnterEM2() or EMU_EnterEM3() with the restore parameter set to true, but it allows the state to be saved without going to sleep. The state can be restored manually by calling EMU_Restore() .
◆ EMU_Restore()
| void EMU_Restore | ( | void | 
            | ) | 
Restore CMU HF clock select state, oscillator enable, and voltage scaling (if available) after EMU_EnterEM2() or EMU_EnterEM3() are called with the restore parameter set to false.
Calling this function is equivalent to calling EMU_EnterEM2() or EMU_EnterEM3() with the restore parameter set to true, but it allows the application to evaluate the wakeup reason before restoring state.
◆ EMU_EM4Init()
| void EMU_EM4Init | ( | const EMU_EM4Init_TypeDef * | 
            em4Init
            | ) | 
Update the EMU module with Energy Mode 4 configuration.
- Parameters
- 
         [in] em4InitEnergy Mode 4 configuration structure. 
◆ EMU_EM4PresleepHook()
| void EMU_EM4PresleepHook | ( | void | 
            | ) | 
Energy mode 4 pre-sleep hook function.
This function is called by EMU_EnterEM4() just prior to the sequence of writes to put the device in EM4. The function implementation does not perform anything, but it is SL_WEAK so that it can be re-implemented in application code if actions are needed.
◆ EMU_EFPEM4PresleepHook()
| void EMU_EFPEM4PresleepHook | ( | void | 
            | ) | 
EFP's Energy mode 4 pre-sleep hook function.
This function is similar to EMU_EM4PresleepHook() but is reserved for EFP usage.
- Note
- The function is primarily meant to be used in systems with EFP circuitry. (EFP = Energy Friendly Pmic (PMIC = Power Management IC)). In such systems there is a need to drive certain signals to EFP pins to notify about energy mode transitions.
◆ EMU_EnterEM4()
| void EMU_EnterEM4 | ( | void | 
            | ) | 
Enter energy mode 4 (EM4).
- Note
- Only a power on reset or external reset pin can wake the device from EM4.
◆ EMU_EnterEM4H()
| void EMU_EnterEM4H | ( | void | 
            | ) | 
Enter energy mode 4 hibernate (EM4H).
- Note
- Retention of clocks and GPIO in EM4 can be configured using EMU_EM4Init before calling this function.
◆ EMU_EnterEM4S()
| void EMU_EnterEM4S | ( | void | 
            | ) | 
Enter energy mode 4 shutoff (EM4S).
- Note
- Retention of clocks and GPIO in EM4 can be configured using EMU_EM4Init before calling this function.
◆ EMU_MemPwrDown()
| void EMU_MemPwrDown | ( | uint32_t | 
            blocks
            | ) | 
Power down memory block.
- Parameters
- 
         [in] blocksSpecifies a logical OR of bits indicating memory blocks to power down. Bit 0 selects block 1, bit 1 selects block 2, and so on. Memory block 0 cannot be disabled. See the reference manual for available memory blocks for a device. 
- Note
- Only a POR reset can power up the specified memory block(s) after power down.
◆ EMU_RamPowerDown()
| void EMU_RamPowerDown | ( | uint32_t | 
            start,
            | 
| uint32_t | 
            end
            | ||
| ) | 
Power down RAM memory blocks.
This function will power down all the RAM blocks that are within a given range. The RAM block layout is different between device families, so this function can be used in a generic way to power down a RAM memory region which is known to be unused.
This function will only power down blocks which are completely enclosed by the memory range given by [start, end).
This is an example to power down all RAM blocks except the first one. The first RAM block is special in that it cannot be powered down by the hardware. The size of the first RAM block is device-specific. See the reference manual to find the RAM block sizes.
- Note
- Only a reset can power up the specified memory block(s) after power down on a series 0 device. The specified memory block(s) will stay off until a call to EMU_RamPowerUp() is done on series 1/2.
- Parameters
- 
         [in] startThe start address of the RAM region to power down. This address is inclusive. [in] endThe end address of the RAM region to power down. This address is exclusive. If this parameter is 0, all RAM blocks contained in the region from start to the upper RAM address will be powered down. 
◆ EMU_RamPowerUp()
| void EMU_RamPowerUp | ( | void | 
            | ) | 
Power up all available RAM memory blocks.
This function will power up all the RAM blocks on a device, this means that the RAM blocks are retained in EM2/EM3. Note that this functionality is not supported on Series 0 devices. Only a reset will power up the RAM blocks on a series 0 device.
◆ EMU_UpdateOscConfig()
| void EMU_UpdateOscConfig | ( | void | 
            | ) | 
Update EMU module with CMU oscillator selection/enable status.
◆ EMU_EFPEM01VScale()
| void EMU_EFPEM01VScale | ( | EMU_VScaleEM01_TypeDef | 
            voltage
            | ) | 
Energy mode 01 voltage scaling hook function.
- Parameters
- 
         [in] voltageVoltage scaling level requested. 
This function is called by EMU_VScaleEM01 to let EFP know that voltage scaling is requested.
◆ EMU_VScaleEM01ByClock()
| void EMU_VScaleEM01ByClock | ( | uint32_t | 
            clockFrequency,
            | 
| bool | 
            wait
            | ||
| ) | 
Voltage scale in EM0 and 1 by clock frequency.
- Parameters
- 
         [in] clockFrequencyUse CMSIS HF clock if 0 or override to custom clock. Providing a custom clock frequency is required if using a non-standard HFXO frequency. [in] waitWait for scaling to complete. 
- Note
- This function is primarily needed by the CMU - Clock Management Unit .
◆ EMU_VScaleEM01()
| void EMU_VScaleEM01 | ( | EMU_VScaleEM01_TypeDef | 
            voltage,
            | 
| bool | 
            wait
            | ||
| ) | 
Force voltage scaling in EM0 and 1 to a specific voltage level.
- Parameters
- 
         [in] voltageTarget VSCALE voltage level. [in] waitWait for scaling to complete. 
- Note
- This function is useful for upscaling before programming Flash from MSC - Memory System Controller and downscaling after programming is done. Flash programming is only supported at emuVScaleEM01_HighPerformance .
- This function ignores vScaleEM01LowPowerVoltageEnable set from EMU_EM01Init() .
◆ EMU_TemperatureGet()
| float EMU_TemperatureGet | ( | void | 
            | ) | 
Get temperature in degrees Celsius.
- Returns
- Temperature in degrees Celsius
◆ EMU_EFPDirectModeEnable()
| void EMU_EFPDirectModeEnable | ( | bool | 
            enable
            | ) | 
Enable/disable EFP Direct Mode.
- Parameters
- 
         [in] enableTrue to enable direct mode. 
◆ EMU_EFPDriveDecoupleSet()
| void EMU_EFPDriveDecoupleSet | ( | bool | 
            enable
            | ) | 
Set to enable EFP to drive Decouple voltage.
Once set, internal LDO will be disabled, and the EMU will control EFP for voltage-scaling. Note that because this bit disables the internal LDO powering the core, it should not be set until after EFP's DECOUPLE output has been configured and enabled.
- Parameters
- 
         [in] enableTrue to enable EFP to drive Decouple voltage. 
◆ EMU_EFPDriveDvddSet()
| void EMU_EFPDriveDvddSet | ( | bool | 
            enable
            | ) | 
Set to enable EFP to drive DVDD voltage.
Set this if EFP's DCDC output is powering DVDD supply. This mode assumes that internal DCDC is not being used.
- Parameters
- 
         [in] enableTrue to enable EFP to drive DVDD voltage. 
◆ EMU_DCDCLock()
| 
 | inline | 
Lock DCDC registers in order to protect them against unintended modification.
◆ EMU_DCDCUnlock()
| 
 | inline | 
Unlock the DCDC so that writing to locked registers again is possible.
◆ EMU_DCDCSync()
| 
 | inline | 
Wait for the DCDC to complete all synchronization of register changes.
- Parameters
- 
         [in] maskA bitmask corresponding to SYNCBUSY register defined bits indicating registers that must complete any ongoing synchronization. 
◆ EMU_EnterEM1()
| 
 | inline | 
Enter energy mode 1 (EM1).
◆ EMU_VScaleWait()
| 
 | inline | 
Wait for voltage scaling to complete.
◆ EMU_VScaleGet()
| 
 | inline | 
Get current voltage scaling level.
- Returns
- Current voltage scaling level.
◆ EMU_IntClear()
| 
 | inline | 
Clear one or more pending EMU interrupts.
- Parameters
- 
         [in] flagsPending EMU interrupt sources to clear. Use one or more valid interrupt flags for the EMU module (EMU_IFC_nnn or EMU_IF_nnn). 
◆ EMU_IntDisable()
| 
 | inline | 
Disable one or more EMU interrupts.
- Parameters
- 
         [in] flagsEMU interrupt sources to disable. Use one or more valid interrupt flags for the EMU module (EMU_IEN_nnn). 
◆ EMU_IntEnable()
| 
 | inline | 
Enable one or more EMU interrupts.
- Note
- Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using EMU_IntClear() prior to enabling the interrupt.
- Parameters
- 
         [in] flagsEMU interrupt sources to enable. Use one or more valid interrupt flags for the EMU module (EMU_IEN_nnn). 
◆ EMU_EFPIntEnable()
| 
 | inline | 
Enable EFP interrupts.
- Parameters
- 
         [in] flagsEnable/disable EFP interrupts. 
◆ EMU_EFPIntGet()
| 
 | inline | 
Get pending EMU EFP interrupt flags.
- Note
- Event bits are not cleared by the use of this function.
- Returns
- EMU EFP interrupt sources pending. .
◆ EMU_EFPIntClear()
| 
 | inline | 
Clear one or more pending EMU EFP interrupts.
- Parameters
- 
         [in] flagsPending EMU EFP interrupt sources to clear. Use one or more valid interrupt flags for the EMU EFP module. 
◆ EMU_IntGet()
| 
 | inline | 
Get pending EMU interrupt flags.
- Note
- Event bits are not cleared by the use of this function.
- Returns
- EMU interrupt sources pending. Returns one or more valid interrupt flags for the EMU module (EMU_IF_nnn).
◆ EMU_IntGetEnabled()
| 
 | inline | 
Get enabled and pending EMU interrupt flags.
Useful for handling more interrupt sources in the same interrupt handler.
- Note
- Interrupt flags are not cleared by the use of this function.
- Returns
- 
         Pending and enabled EMU interrupt sources Return value is the bitwise AND of
         - the enabled interrupt sources in EMU_IEN and
- the pending interrupt flags EMU_IF.
 
◆ EMU_IntSet()
| 
 | inline | 
Set one or more pending EMU interrupts.
- Parameters
- 
         [in] flagsEMU interrupt sources to set to pending. Use one or more valid interrupt flags for the EMU module (EMU_IFS_nnn). 
◆ EMU_Lock()
| 
 | inline | 
Lock EMU registers in order to protect them against unintended modification.
- Note
- If locking EMU registers, they must be unlocked prior to using any EMU API functions modifying EMU registers, excluding interrupt control and regulator control if the architecture has a EMU_PWRCTRL register. An exception to this is the energy mode entering API (EMU_EnterEMn()), which can be used when the EMU registers are locked.
◆ EMU_Unlock()
| 
 | inline | 
Unlock the EMU so that writing to locked registers again is possible.
◆ EMU_UnlatchPinRetention()
| 
 | inline | 
When EM4 pin retention is set to emuPinRetentionLatch, then pins are retained through EM4 entry and wakeup.
The pin state is released by calling this function. The feature allows peripherals or GPIO to be re-initialized after EM4 exit (reset), and when initialization is done, this function can release pins and return control to the peripherals or GPIO.
◆ EMU_TemperatureReady()
| 
 | inline | 
Temperature measurement ready status.
- Returns
- True if temperature measurement is ready
◆ EMU_TemperatureAvgGet()
| 
 | inline | 
Get averaged temperature in degrees Celsius.
- Note
- An averaged temperature measurement must first be requested by calling EMU_TemperatureAvgRequest() and waiting for the TEMPAVG interrupt flag to go high.
- Returns
- Averaged temperature
◆ EMU_TemperatureAvgRequest()
| 
 | inline | 
Request averaged temperature.
- Note
- EMU must be unlocked by calling EMU_Unlock() before this function can be called.
- Parameters
- 
         [in] numSamplesNumber of temperature samples to average 
Macro Definition Documentation
◆ EMU_VSCALE_PRESENT
| #define EMU_VSCALE_PRESENT | 
Voltage scaling present.
◆ EMU_VSCALE_EM01_PRESENT
| #define EMU_VSCALE_EM01_PRESENT | 
Voltage scaling for EM01 present.
◆ EMU_EM01INIT_DEFAULT
| #define EMU_EM01INIT_DEFAULT | 
Default initialization of EM0 and 1 configuration.
◆ EMU_EM23INIT_DEFAULT
| #define EMU_EM23INIT_DEFAULT | 
Default initialization of EM2 and 3 configuration.
◆ EMU_EM4INIT_DEFAULT
| #define EMU_EM4INIT_DEFAULT | 
Default initialization of EM4 configuration (Series 1 without VSCALE).
◆ EMU_TEMP_ZERO_C_IN_KELVIN
| #define EMU_TEMP_ZERO_C_IN_KELVIN (273.15f) | 
Zero degrees Celcius in Kelvin.
Enumeration Type Documentation
◆ EMU_BODMode_TypeDef
| enum EMU_BODMode_TypeDef | 
◆ EMU_EM4State_TypeDef
| enum EMU_EM4State_TypeDef | 
◆ EMU_EM4PinRetention_TypeDef
EM4 Pin Retention Type.
| Enumerator | |
|---|---|
| emuPinRetentionDisable | No Retention: Pads enter reset state when entering EM4. | 
| emuPinRetentionEm4Exit | Retention through EM4: Pads enter reset state when exiting EM4. | 
| emuPinRetentionLatch | Retention through EM4 and wakeup: call EMU_UnlatchPinRetention() to release pins from retention after EM4 wakeup. | 
◆ EMU_PowerConfig_TypeDef
◆ EMU_VScaleEM01_TypeDef
Supported EM0/1 Voltage Scaling Levels.
| Enumerator | |
|---|---|
| emuVScaleEM01_HighPerformance | High-performance voltage level. HF clock can be set to any frequency. | 
| emuVScaleEM01_LowPower | Low-power optimized voltage level. HF clock must be limited to CMU_VSCALEEM01_LOWPOWER_VOLTAGE_CLOCK_MAX Hz at this voltage. EM0/1 voltage scaling is applied when core clock frequency is changed from CMU - Clock Management Unit or when calling EMU_EM01Init() when HF clock is already below the limit. Minimum VSCALE level in EM0/1 is VSCALE1. | 
◆ EMU_VScaleEM23_TypeDef
Supported EM2/3 Voltage Scaling Levels.