ACMP_Init_TypeDef Struct Reference
ACMP initialization structure.
      
       #include <em_acmp.h>
      
     
| Data Fields | |
| uint32_t | biasProg | 
| Bias current. | |
| ACMP_InputRange_TypeDef | inputRange | 
| Input range. | |
| ACMP_Accuracy_TypeDef | accuracy | 
| ACMP accuracy mode. | |
| ACMP_HysteresisLevel_TypeDef | hysteresisLevel | 
| Hysteresis level. | |
| bool | inactiveValue | 
| Inactive value emitted by ACMP during warmup. | |
| uint32_t | vrefDiv | 
| VDD division factor. | |
| bool | enable | 
| If true, ACMP is enabled after configuration. | |
ACMP initialization structure.
Field Documentation
◆ biasProg
| uint32_t ACMP_Init_TypeDef::biasProg | 
Bias current.
See the ACMP chapter about bias and response time in the reference manual for details. Valid values are in the range 0-7.
◆ inputRange
| ACMP_InputRange_TypeDef ACMP_Init_TypeDef::inputRange | 
Input range.
        Adjust this setting to optimize the performance for a given input voltage range.
        
       
◆ accuracy
| ACMP_Accuracy_TypeDef ACMP_Init_TypeDef::accuracy | 
ACMP accuracy mode.
Select the accuracy mode that matches the required current usage and accuracy requirement. Low accuracy consumes less current while high accuracy consumes more current.
◆ hysteresisLevel
| ACMP_HysteresisLevel_TypeDef ACMP_Init_TypeDef::hysteresisLevel | 
Hysteresis level.
◆ inactiveValue
| bool ACMP_Init_TypeDef::inactiveValue | 
Inactive value emitted by ACMP during warmup.
◆ vrefDiv
| uint32_t ACMP_Init_TypeDef::vrefDiv | 
VDD division factor.
VREFOUT = VREFIN * (VREFDIV / 63). Valid values are in the 0-63 range.
◆ enable
| bool ACMP_Init_TypeDef::enable | 
If true, ACMP is enabled after configuration.