SE_Command_t Struct Reference
SE Command structure to which all commands to the SE must adhere.
      
       #include <em_se.h>
      
     
| Data Fields | |
| uint32_t | command | 
| SE Command. | |
| SE_DataTransfer_t * | data_in | 
| Input data. | |
| SE_DataTransfer_t * | data_out | 
| Output data. | |
| uint32_t | parameters [ SE_MAX_PARAMETERS ] | 
| Parameters. | |
| size_t | num_parameters | 
| Number of parameters. | |
SE Command structure to which all commands to the SE must adhere.
Field Documentation
◆ command
| uint32_t SE_Command_t::command | 
SE Command.
◆ data_in
| SE_DataTransfer_t * SE_Command_t::data_in | 
Input data.
◆ data_out
| SE_DataTransfer_t * SE_Command_t::data_out | 
Output data.
◆ parameters
| uint32_t SE_Command_t::parameters[ SE_MAX_PARAMETERS ] | 
Parameters.
◆ num_parameters
| size_t SE_Command_t::num_parameters | 
Number of parameters.