Common BSP for all kitsBSP

Macros

#define BSP_INIT_BCC   0x04
 
#define BSP_INIT_DK_EBI   0x02
 
#define BSP_INIT_DK_SPI   0x01
 
#define BSP_INIT_IOEXP   0x08
 
#define BSP_STATUS_ILLEGAL_PARAM   (-1)
 
#define BSP_STATUS_IOEXP_FAILURE   (-4)
 
#define BSP_STATUS_NOT_IMPLEMENTED   (-2)
 
#define BSP_STATUS_OK   0
 
#define BSP_STATUS_UNSUPPORTED_MODE   (-3)
 

Functions

int BSP_Disable (void)
 Deinitialize board support package functionality. Reverse actions performed by BSP_Init(). This function is a dummy on STK's.
 
int BSP_Init (uint32_t flags)
 Initialize board support package functionality.
 
int BSP_LedClear (int ledNo)
 Turn off a single LED.
 
int BSP_LedGet (int ledNo)
 Get current status of a single LED.
 
int BSP_LedSet (int ledNo)
 Turn on a single LED.
 
uint32_t BSP_LedsGet (void)
 Get status of all LEDs.
 
int BSP_LedsInit (void)
 Initialize LED drivers.
 
int BSP_LedsSet (uint32_t leds)
 Update all LED's.
 
int BSP_LedToggle (int ledNo)
 Toggle a single LED.
 
int BSP_PeripheralAccess (BSP_Peripheral_TypeDef perf, bool enable)
 DK Peripheral Access Control Enable or disable access to on-board peripherals through switches and SPI switch where applicable. Turn off conflicting peripherals when enabling another.
 
bool BSP_TraceProfilerSetup (void)
 Configure SWO trace output for Energy Profiler.
 
void BSP_TraceSwoSetup (void)
 Energy Profiler SWO setup.
 

Macro Definition Documentation

#define BSP_INIT_BCC   0x04

Mode flag for BSP_Init(), init board controller communication.

Definition at line 56 of file bsp.h.

#define BSP_INIT_DK_EBI   0x02

Mode flag for BSP_Init(), init DK in EBI mode (DK3x50 only).

Definition at line 55 of file bsp.h.

Referenced by BSP_Disable(), BSP_Init(), BSP_RegisterRead(), and BSP_RegisterWrite().

#define BSP_INIT_DK_SPI   0x01

Mode flag for BSP_Init(), init DK in SPI mode (DK3x50 only).

Definition at line 54 of file bsp.h.

Referenced by BSP_Disable(), and BSP_Init().

#define BSP_INIT_IOEXP   0x08

Mode flag for BSP_Init(), init io-expander on some radio boards

Definition at line 57 of file bsp.h.

Referenced by BSP_initBoard().

#define BSP_STATUS_ILLEGAL_PARAM   (-1)

BSP API return code, illegal input parameter.

Definition at line 48 of file bsp.h.

Referenced by BSP_BusControlModeSet(), BSP_LedClear(), BSP_LedGet(), BSP_LedSet(), and BSP_LedToggle().

#define BSP_STATUS_IOEXP_FAILURE   (-4)

BSP API return code, io-expander communication failed

Definition at line 51 of file bsp.h.

#define BSP_STATUS_NOT_IMPLEMENTED   (-2)

BSP API return code, function not implemented (dummy).

Definition at line 49 of file bsp.h.

Referenced by BSP_EbiDeInit(), BSP_EbiInit(), BSP_McuBoard_UsbStatusLedEnable(), and BSP_McuBoard_UsbVbusPowerEnable().

#define BSP_STATUS_UNSUPPORTED_MODE   (-3)

BSP API return code, unsupported BSP mode.

Definition at line 50 of file bsp.h.

Function Documentation

int BSP_Disable ( void  )

Deinitialize board support package functionality. Reverse actions performed by BSP_Init(). This function is a dummy on STK's.

Returns
BSP_STATUS_OK on DK's, BSP_STATUS_NOT_IMPLEMENTED on STK's.

Definition at line 93 of file bsp_dk_3201.c.

References BSP_BusControl_OFF, BSP_BusControlModeSet(), BSP_INIT_DK_EBI, BSP_INIT_DK_SPI, and BSP_STATUS_OK.

int BSP_Init ( uint32_t  flags)

Initialize board support package functionality.

Parameters
[in]flagsDK3x50: Initialize in EBI or SPI mode using BSP_INIT_DK_EBI or BSP_INIT_DK_SPI. Gxxx_DK: Use 0. STK: Use BSP_INIT_BCC to initialize board controller UART, 0 otherwise.

The value BSP_INIT_DEFAULT is defined and is: BSP_INIT_DK_EBI on DK3x50, 0 on all other kits.

Returns
BSP_STATUS_OK

Definition at line 121 of file bsp_dk_3201.c.

References BC_REGISTER, BSP_BusControl_EBI, BSP_BusControl_SPI, BSP_BusControlModeSet(), BSP_INIT_DK_EBI, BSP_INIT_DK_SPI, BSP_RegisterRead(), BSP_RegisterWrite(), and BSP_STATUS_OK.

Referenced by BSP_initBoard().

int BSP_LedClear ( int  ledNo)

Turn off a single LED.

Parameters
[in]ledNoThe number of the LED (counting from zero) to turn off.
Returns
BSP_STATUS_OK or BSP_STATUS_ILLEGAL_PARAM if illegal LED number.

Definition at line 70 of file bsp_dk_leds.c.

References BSP_RegisterRead(), BSP_RegisterWrite(), BSP_STATUS_ILLEGAL_PARAM, and BSP_STATUS_OK.

int BSP_LedGet ( int  ledNo)

Get current status of a single LED.

Parameters
[in]ledNoThe number of the LED (counting from zero) to check.
Returns
1 if LED is on, 0 if LED is off, BSP_STATUS_ILLEGAL_PARAM if illegal LED number.

Definition at line 90 of file bsp_dk_leds.c.

References BSP_RegisterRead(), and BSP_STATUS_ILLEGAL_PARAM.

int BSP_LedSet ( int  ledNo)

Turn on a single LED.

Parameters
[in]ledNoThe number of the LED (counting from zero) to turn on.
Returns
BSP_STATUS_OK or BSP_STATUS_ILLEGAL_PARAM if illegal LED number.

Definition at line 108 of file bsp_dk_leds.c.

References BSP_RegisterRead(), BSP_RegisterWrite(), BSP_STATUS_ILLEGAL_PARAM, and BSP_STATUS_OK.

uint32_t BSP_LedsGet ( void  )

Get status of all LEDs.

Returns
Bitmask with current status for all LED's.

Definition at line 46 of file bsp_dk_leds.c.

References BSP_RegisterRead().

int BSP_LedsInit ( void  )

Initialize LED drivers.

Note
LED's are initially turned off.
Returns
BSP_STATUS_OK

Definition at line 35 of file bsp_dk_leds.c.

References BSP_RegisterWrite(), and BSP_STATUS_OK.

Referenced by BSP_initBoard().

int BSP_LedsSet ( uint32_t  leds)

Update all LED's.

Parameters
[in]ledsBitmask representing new status for all LED's. A 1 turns a LED on, a 0 turns a LED off.
Returns
BSP_STATUS_OK

Definition at line 58 of file bsp_dk_leds.c.

References BSP_RegisterWrite(), and BSP_STATUS_OK.

int BSP_LedToggle ( int  ledNo)

Toggle a single LED.

Parameters
[in]ledNoThe number of the LED (counting from zero) to toggle.
Returns
BSP_STATUS_OK or BSP_STATUS_ILLEGAL_PARAM if illegal LED number.

Definition at line 127 of file bsp_dk_leds.c.

References BSP_RegisterRead(), BSP_RegisterWrite(), BSP_STATUS_ILLEGAL_PARAM, and BSP_STATUS_OK.

int BSP_PeripheralAccess ( BSP_Peripheral_TypeDef  perf,
bool  enable 
)

DK Peripheral Access Control Enable or disable access to on-board peripherals through switches and SPI switch where applicable. Turn off conflicting peripherals when enabling another.

Parameters
[in]perfWhich peripheral to configure. Use enum BSP_Peripheral_TypeDef or BSP_Peripheral_Typedef according to DK type.
[in]enableIf true, set up access to peripheral, if false disable access.
Returns
BSP_STATUS_OK.

Definition at line 443 of file bsp_dk_3201.c.

References BC_PERICON_ANALOG_DIFF_SHIFT, BC_PERICON_ANALOG_SE_SHIFT, BC_PERICON_AUDIO_IN_SHIFT, BC_PERICON_AUDIO_OUT_SEL_SHIFT, BC_PERICON_AUDIO_OUT_SHIFT, BC_PERICON_I2C_SHIFT, BC_PERICON_I2S_ETH_SEL_SHIFT, BC_PERICON_I2S_ETH_SHIFT, BC_PERICON_RS232_LEUART_SHIFT, BC_PERICON_RS232_SHUTDOWN_SHIFT, BC_PERICON_RS232_UART_SHIFT, BC_PERICON_SPI_SHIFT, BC_PERICON_TOUCH_SHIFT, BC_PERICON_TRACE_SHIFT, BC_REGISTER, BSP_ANALOG_DIFF, BSP_ANALOG_SE, BSP_AUDIO_IN, BSP_AUDIO_OUT, BSP_ETH, BSP_I2C, BSP_I2S, BSP_MICROSD, BSP_RegisterRead(), BSP_RegisterWrite(), BSP_RS232_LEUART, BSP_RS232_SHUTDOWN, BSP_RS232_UART, BSP_STATUS_OK, BSP_TFT, BSP_TOUCH, and BSP_TRACE.

Referenced by BSP_initBoard(), TFT_DirectInit(), and TOUCH_Init().

bool BSP_TraceProfilerSetup ( void  )

Configure SWO trace output for Energy Profiler.

Note
Enabling SWO trace will add ~150uA current consumption in EM0.
Returns
Always true

Definition at line 95 of file bsp_trace.c.

References _GPIO_ROUTE_SWLOCATION_MASK, CMU, CMU_ClockFreqGet(), CMU_HFPERCLKEN0_GPIO, CMU_OSCENCMD_AUXHFRCOEN, CMU_STATUS_AUXHFRCORDY, cmuClock_DBG, GPIO, and GPIO_ROUTE_SWOPEN.

Referenced by BSP_TraceSwoSetup().

void BSP_TraceSwoSetup ( void  )

Energy Profiler SWO setup.

Deprecated:
Deprecated function. New code should call BSP_TraceProfilerSetup().

Definition at line 164 of file bsp_trace.c.

References BSP_TraceProfilerSetup().

Referenced by RETARGET_SwoInit().