LESENSE_Init_TypeDef Struct ReferenceEMLIB > LESENSE
LESENSE module initialization structure.
Definition at line 738
of file em_lesense.h
.
#include <
em_lesense.h
>
Data Fields | |
LESENSE_CoreCtrlDesc_TypeDef | coreCtrl |
LESENSE_DecCtrlDesc_TypeDef | decCtrl |
LESENSE_PerCtrlDesc_TypeDef | perCtrl |
LESENSE_TimeCtrlDesc_TypeDef | timeCtrl |
Field Documentation
LESENSE_CoreCtrlDesc_TypeDef LESENSE_Init_TypeDef::coreCtrl |
LESENSE core configuration parameters.
Definition at line 740
of file em_lesense.h
.
Referenced by CAPLESENSE_setupLESENSE(), and LESENSE_Init().
LESENSE_DecCtrlDesc_TypeDef LESENSE_Init_TypeDef::decCtrl |
LESENSE decoder configuration parameters.
Definition at line 749
of file em_lesense.h
.
Referenced by LESENSE_Init().
LESENSE_PerCtrlDesc_TypeDef LESENSE_Init_TypeDef::perCtrl |
LESENSE peripheral configuration parameters.
Definition at line 746
of file em_lesense.h
.
Referenced by LESENSE_Init().
LESENSE_TimeCtrlDesc_TypeDef LESENSE_Init_TypeDef::timeCtrl |
LESENSE timing configuration parameters.
Definition at line 743
of file em_lesense.h
.
Referenced by LESENSE_Init().
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/emlib/inc/
em_lesense.h