AES_TypeDef Struct ReferenceDevices > EFM32GG_AES
Definition at line 48
of file efm32gg_aes.h
.
Data Fields | |
__IOM uint32_t | CMD |
__IOM uint32_t | CTRL |
__IOM uint32_t | DATA |
__IOM uint32_t | IEN |
__IM uint32_t | IF |
__IOM uint32_t | IFC |
__IOM uint32_t | IFS |
__IOM uint32_t | KEYHA |
__IOM uint32_t | KEYHB |
__IOM uint32_t | KEYHC |
__IOM uint32_t | KEYHD |
__IOM uint32_t | KEYLA |
__IOM uint32_t | KEYLB |
__IOM uint32_t | KEYLC |
__IOM uint32_t | KEYLD |
uint32_t | RESERVED0 [3] |
__IM uint32_t | STATUS |
__IOM uint32_t | XORDATA |
Field Documentation
__IOM uint32_t AES_TypeDef::CMD |
Command Register
Definition at line 50
of file efm32gg_aes.h
.
__IOM uint32_t AES_TypeDef::CTRL |
Control Register
Definition at line 49
of file efm32gg_aes.h
.
__IOM uint32_t AES_TypeDef::DATA |
DATA Register
Definition at line 56
of file efm32gg_aes.h
.
__IOM uint32_t AES_TypeDef::IEN |
Interrupt Enable Register
Definition at line 52
of file efm32gg_aes.h
.
__IM uint32_t AES_TypeDef::IF |
Interrupt Flag Register
Definition at line 53
of file efm32gg_aes.h
.
__IOM uint32_t AES_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line 55
of file efm32gg_aes.h
.
__IOM uint32_t AES_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line 54
of file efm32gg_aes.h
.
__IOM uint32_t AES_TypeDef::KEYHA |
KEY High Register
Definition at line 63
of file efm32gg_aes.h
.
__IOM uint32_t AES_TypeDef::KEYHB |
KEY High Register
Definition at line 64
of file efm32gg_aes.h
.
__IOM uint32_t AES_TypeDef::KEYHC |
KEY High Register
Definition at line 65
of file efm32gg_aes.h
.
__IOM uint32_t AES_TypeDef::KEYHD |
KEY High Register
Definition at line 66
of file efm32gg_aes.h
.
__IOM uint32_t AES_TypeDef::KEYLA |
KEY Low Register
Definition at line 59
of file efm32gg_aes.h
.
__IOM uint32_t AES_TypeDef::KEYLB |
KEY Low Register
Definition at line 60
of file efm32gg_aes.h
.
__IOM uint32_t AES_TypeDef::KEYLC |
KEY Low Register
Definition at line 61
of file efm32gg_aes.h
.
__IOM uint32_t AES_TypeDef::KEYLD |
KEY Low Register
Definition at line 62
of file efm32gg_aes.h
.
uint32_t AES_TypeDef::RESERVED0[3] |
Reserved for future use
Definition at line 58
of file efm32gg_aes.h
.
__IM uint32_t AES_TypeDef::STATUS |
Status Register
Definition at line 51
of file efm32gg_aes.h
.
__IOM uint32_t AES_TypeDef::XORDATA |
XORDATA Register
Definition at line 57
of file efm32gg_aes.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32GG/Include/
efm32gg_aes.h