MSCEMLIB
Detailed Description
Memory System Controller API.
This module contain functions to control the MSC, primarily the Flash. The user can perform Flash memory write and erase operations as well as optimization of the CPU instruction fetch interface for the application. Available instruction fetch features depends on the MCU or SoC family, but features such as instruction pre-fetch, cache and configurable branch prediction are typically available.
- Note
- Flash wait-state configuration is handled by the CMU module. When the core clock configuration is changed by a calls to functions such as CMU_ClockSelectSet() or CMU_HFRCOBandSet() , then Flash wait-state configuration is also updated.
The MSC resets into a safe state. To initialize the instruction interface to recommended settings:
- Note
- The optimal configuration is highly application dependent. Performance benchmarking is supported by most families. See MSC_StartCacheMeasurement() and MSC_GetCacheMeasurement() for more details.
Support for Flash write and erase runs from RAM by default. This code may be allocated to Flash by defining EM_MSC_RUN_FROM_FLASH .
- Note
- Flash erase may add ms of delay to interrupt latency if executing from Flash.
Flash write and erase operations are supported by MSC_WriteWord() , MSC_WriteWordFast() , MSC_ErasePage() and MSC_MassErase() . Fast write is not supported for EFM32G and mass erase is supported for MCU and SoC families with larger Flash sizes.
- Note
- MSC_Init() must be called prior to any Flash write or erase operation.
The following steps are necessary to perform a page erase and write:
Data Structures |
|
| struct | MSC_ExecConfig_TypeDef |
Macros |
|
| #define | EM_MSC_RUN_FROM_FLASH |
|
By compiling with the define EM_MSC_RUN_FROM_FLASH, the functions performing erase or write operations will remain in and execute from Flash. This is useful for targets that don't want to allocate RAM space to hold the flash functions. Without this define, code for Flash operations will be copied into RAM at startup.
|
|
| #define | MSC_EXECCONFIG_DEFAULT |
| #define | MSC_PROGRAM_TIMEOUT 10000000ul |
|
The timeout used while waiting for the flash to become ready after a write. This number indicates the number of iterations to perform before issuing a timeout.
|
|
| #define | MSC_RAMFUNC_DECLARATOR |
|
Expands to
SL_RAMFUNC_DECLARATOR
if
EM_MSC_RUN_FROM_FLASH
is undefined and to nothing if
EM_MSC_RUN_FROM_FLASH
is defined.
|
|
| #define | MSC_RAMFUNC_DEFINITION_BEGIN |
|
Expands to
SL_RAMFUNC_DEFINITION_BEGIN
if
EM_MSC_RUN_FROM_FLASH
is undefined and to nothing if
EM_MSC_RUN_FROM_FLASH
is defined.
|
|
| #define | MSC_RAMFUNC_DEFINITION_END |
|
Expands to
SL_RAMFUNC_DEFINITION_END
if
EM_MSC_RUN_FROM_FLASH
is undefined and to nothing if
EM_MSC_RUN_FROM_FLASH
is defined.
|
|
Enumerations |
|
| enum |
MSC_BusStrategy_Typedef
{
mscBusStrategyCPU = MSC_READCTRL_BUSSTRATEGY_CPU, mscBusStrategyDMA = MSC_READCTRL_BUSSTRATEGY_DMA, mscBusStrategyDMAEM1 = MSC_READCTRL_BUSSTRATEGY_DMAEM1, mscBusStrategyNone = MSC_READCTRL_BUSSTRATEGY_NONE } |
| enum |
MSC_Status_TypeDef
{
mscReturnOk = 0, mscReturnInvalidAddr = -1, mscReturnLocked = -2, mscReturnTimeOut = -3, mscReturnUnaligned = -4 } |
Functions |
|
| __STATIC_INLINE void | MSC_BusStrategy (mscBusStrategy_Typedef mode) |
|
Configure which unit should get priority on system bus.
|
|
| void | MSC_Deinit (void) |
|
Disables the flash controller for writing.
|
|
| __STATIC_INLINE void | MSC_EnableAutoCacheFlush (bool enable) |
|
Enable or disable instruction cache flushing when writing to flash.
|
|
| __STATIC_INLINE void | MSC_EnableCache (bool enable) |
|
Enable or disable instruction cache functionality.
|
|
| __STATIC_INLINE void | MSC_EnableCacheIRQs (bool enable) |
|
Enable or disable instruction cache functionality in IRQs.
|
|
| MSC_RAMFUNC_DECLARATOR MSC_Status_TypeDef | MSC_ErasePage (uint32_t *startAddress) |
|
Erases a page in flash memory.
|
|
| void | MSC_ExecConfigSet ( MSC_ExecConfig_TypeDef *execConfig) |
|
Set MSC code execution configuration.
|
|
| __STATIC_INLINE void | MSC_FlushCache (void) |
|
Flush the contents of the instruction cache.
|
|
| __STATIC_INLINE int32_t | MSC_GetCacheMeasurement (void) |
|
Stops measuring the hit rate.
|
|
| void | MSC_Init (void) |
|
Enables the flash controller for writing.
|
|
| __STATIC_INLINE void | MSC_IntClear (uint32_t flags) |
|
Clear one or more pending MSC interrupts.
|
|
| __STATIC_INLINE void | MSC_IntDisable (uint32_t flags) |
|
Disable one or more MSC interrupts.
|
|
| __STATIC_INLINE void | MSC_IntEnable (uint32_t flags) |
|
Enable one or more MSC interrupts.
|
|
| __STATIC_INLINE uint32_t | MSC_IntGet (void) |
|
Get pending MSC interrupt flags.
|
|
| __STATIC_INLINE uint32_t | MSC_IntGetEnabled (void) |
|
Get enabled and pending MSC interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
|
|
| __STATIC_INLINE void | MSC_IntSet (uint32_t flags) |
|
Set one or more pending MSC interrupts from SW.
|
|
| MSC_RAMFUNC_DECLARATOR MSC_Status_TypeDef | MSC_MassErase (void) |
|
Erase entire flash in one operation.
|
|
| __STATIC_INLINE void | MSC_StartCacheMeasurement (void) |
|
Starts measuring cache hit ratio.
|
|
| MSC_RAMFUNC_DECLARATOR MSC_Status_TypeDef | MSC_WriteWord (uint32_t *address, void const *data, uint32_t numBytes) |
|
Writes data to flash memory. This function is interrupt safe, but slower than
MSC_WriteWordFast()
, which writes to flash with interrupts disabled. Write data must be aligned to words and contain a number of bytes that is divisable by four.
|
|
| MSC_RAMFUNC_DECLARATOR MSC_Status_TypeDef | MSC_WriteWordFast (uint32_t *address, void const *data, uint32_t numBytes) |
|
Writes data to flash memory. This function is faster than
MSC_WriteWord()
, but it disables interrupts. Write data must be aligned to words and contain a number of bytes that is divisable by four.
|
|
Macro Definition Documentation
| #define EM_MSC_RUN_FROM_FLASH |
By compiling with the define EM_MSC_RUN_FROM_FLASH, the functions performing erase or write operations will remain in and execute from Flash. This is useful for targets that don't want to allocate RAM space to hold the flash functions. Without this define, code for Flash operations will be copied into RAM at startup.
- Note
- This define is not present by default. The MSC controller API will run from RAM by default.
Definition at line
125
of file
em_msc.h
.
| #define MSC_EXECCONFIG_DEFAULT |
Default MSC ExecConfig initialization
Definition at line
162
of file
em_msc.h
.
| #define MSC_PROGRAM_TIMEOUT 10000000ul |
The timeout used while waiting for the flash to become ready after a write. This number indicates the number of iterations to perform before issuing a timeout.
- Note
- This timeout is set very large (in the order of 100x longer than necessary). This is to avoid any corner cases.
Definition at line
110
of file
em_msc.h
.
Referenced by MSC_ErasePage() .
Enumeration Type Documentation
| enum MSC_Status_TypeDef |
Return codes for writing/erasing the flash
Definition at line
133
of file
em_msc.h
.
Function Documentation
| __STATIC_INLINE void MSC_BusStrategy | ( | mscBusStrategy_Typedef |
mode
|
) |
Configure which unit should get priority on system bus.
- Parameters
-
[in] modeUnit to prioritize bus accesses for.
Definition at line
449
of file
em_msc.h
.
References _MSC_READCTRL_BUSSTRATEGY_MASK , and MSC .
| __STATIC_INLINE void MSC_EnableAutoCacheFlush | ( | bool |
enable
|
) |
Enable or disable instruction cache flushing when writing to flash.
- Parameters
-
[in] enableEnable automatic cache flushing. Default is on.
Definition at line
436
of file
em_msc.h
.
References _MSC_READCTRL_AIDIS_SHIFT , BUS_RegBitWrite() , and MSC .
| __STATIC_INLINE void MSC_EnableCache | ( | bool |
enable
|
) |
Enable or disable instruction cache functionality.
- Parameters
-
[in] enableEnable instruction cache. Default is on.
Definition at line
412
of file
em_msc.h
.
References _MSC_READCTRL_IFCDIS_SHIFT , BUS_RegBitWrite() , and MSC .
| __STATIC_INLINE void MSC_EnableCacheIRQs | ( | bool |
enable
|
) |
Enable or disable instruction cache functionality in IRQs.
- Parameters
-
[in] enableEnable instruction cache. Default is on.
Definition at line
424
of file
em_msc.h
.
References _MSC_READCTRL_ICCDIS_SHIFT , BUS_RegBitWrite() , and MSC .
| MSC_RAMFUNC_DEFINITION_BEGIN MSC_Status_TypeDef MSC_ErasePage | ( | uint32_t * |
startAddress
|
) |
Erases a page in flash memory.
- Note
- It is recommended to run this code from RAM. On the Gecko family, it is required to run this function from RAM.
For IAR, Rowley, SimplicityStudio, Atollic and armgcc this will be achieved automatically by using attributes in the function proctype. For Keil uVision you must define a section called "ram_code" and place this manually in your project's scatter file.
- Parameters
-
[in] startAddressPointer to the flash page to erase. Must be aligned to beginning of page boundary.
- Returns
-
Returns the status of erase operation,
MSC_Status_TypeDef
* mscReturnOk - Operation completed successfully. * mscReturnInvalidAddr - Operation tried to erase a non-flash area. * mscReturnLocked - Operation tried to erase a locked area of the flash. * mscReturnTimeOut - Operation timed out waiting for flash operation * to complete. *
Definition at line
975
of file
em_msc.c
.
References EMU , FLASH_PAGE_SIZE , MSC , MSC_PROGRAM_TIMEOUT , MSC_STATUS_BUSY , MSC_STATUS_INVADDR , MSC_STATUS_LOCKED , MSC_WRITECMD_ERASEPAGE , MSC_WRITECMD_LADDRIM , MSC_WRITECTRL_WREN , mscReturnInvalidAddr , mscReturnLocked , mscReturnOk , and mscReturnTimeOut .
Referenced by nvm3_halPageErase() , and NVMHAL_PageErase() .
| void MSC_ExecConfigSet | ( | MSC_ExecConfig_TypeDef * |
execConfig
|
) |
Set MSC code execution configuration.
- Parameters
-
[in] execConfigCode execution configuration
Definition at line
291
of file
em_msc.c
.
References _MSC_READCTRL_MODE_MASK , MSC_ExecConfig_TypeDef::aiDis , MSC_ExecConfig_TypeDef::iccDis , MSC_ExecConfig_TypeDef::ifcDis , MSC , MSC_READCTRL_AIDIS , MSC_READCTRL_ICCDIS , MSC_READCTRL_IFCDIS , MSC_READCTRL_MODE_WS0 , MSC_READCTRL_MODE_WS0SCBTP , MSC_READCTRL_MODE_WS1 , MSC_READCTRL_MODE_WS1SCBTP , MSC_READCTRL_PREFETCH , MSC_ExecConfig_TypeDef::prefetchEn , MSC_ExecConfig_TypeDef::scbtEn , and MSC_ExecConfig_TypeDef::useHprot .
| __STATIC_INLINE int32_t MSC_GetCacheMeasurement | ( | void |
|
) |
Stops measuring the hit rate.
- Note
-
This function is defined inline to minimize the impact of this code on the measurement itself. This code only works for relatively short sections of code. If you wish to measure longer sections of code you need to implement a IRQ Handler for The CHOF and CMOF overflow interrupts. Theses overflows needs to be counted and included in the total. The functions can then be implemented as follows:
* volatile uint32_t hitOverflows * volatile uint32_t missOverflows * * void MSC_IRQHandler(void) * { * uint32_t flags; * flags = MSC->IF; * if (flags & MSC_IF_CHOF) { * MSC->IFC = MSC_IF_CHOF; * hitOverflows++; * } * if (flags & MSC_IF_CMOF) { * MSC->IFC = MSC_IF_CMOF; * missOverflows++; * } * } * * void startPerformanceCounters(void) * { * hitOverflows = 0; * missOverflows = 0; * * MSC_IntEnable(MSC_IF_CHOF | MSC_IF_CMOF); * NVIC_EnableIRQ(MSC_IRQn); * * MSC_StartCacheMeasurement(); * } *
- Returns
- Returns -1 if there has been no cache accesses. Returns -2 if there has been an overflow in the performance counters. If not, it will return the percentage of hits versus misses.
Definition at line
366
of file
em_msc.h
.
References MSC , MSC_CMD_STOPPC , MSC_IF_CHOF , and MSC_IF_CMOF .
| void MSC_Init | ( | void |
|
) |
Enables the flash controller for writing.
- Note
- This function must be called before flash operations when AUXHFRCO clock has been changed from default band.
Definition at line
225
of file
em_msc.c
.
References _MSC_TIMEBASE_BASE_MASK , _MSC_TIMEBASE_BASE_SHIFT , _MSC_TIMEBASE_PERIOD_MASK , CMU_ClockFreqGet() , cmuClock_AUX , EMU , MSC , MSC_TIMEBASE_PERIOD_1US , MSC_TIMEBASE_PERIOD_5US , MSC_UNLOCK_CODE , and MSC_WRITECTRL_WREN .
Referenced by nvm3_halOpen() , and NVMHAL_Init() .
| __STATIC_INLINE void MSC_IntClear | ( | uint32_t |
flags
|
) |
Clear one or more pending MSC interrupts.
- Parameters
-
[in] flagsPending MSC intterupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for the MSC module (MSC_IF_nnn).
Definition at line
213
of file
em_msc.h
.
References MSC .
| __STATIC_INLINE void MSC_IntDisable | ( | uint32_t |
flags
|
) |
Disable one or more MSC interrupts.
- Parameters
-
[in] flagsMSC interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for the MSC module (MSC_IF_nnn).
Definition at line
226
of file
em_msc.h
.
References MSC .
| __STATIC_INLINE void MSC_IntEnable | ( | uint32_t |
flags
|
) |
Enable one or more MSC interrupts.
- Note
- Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. Consider using MSC_IntClear() prior to enabling if such a pending interrupt should be ignored.
- Parameters
-
[in] flagsMSC interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for the MSC module (MSC_IF_nnn).
Definition at line
244
of file
em_msc.h
.
References MSC .
| __STATIC_INLINE uint32_t MSC_IntGet | ( | void |
|
) |
Get pending MSC interrupt flags.
- Note
- The event bits are not cleared by the use of this function.
- Returns
- MSC interrupt sources pending. A bitwise logic OR combination of valid interrupt flags for the MSC module (MSC_IF_nnn).
Definition at line
260
of file
em_msc.h
.
References MSC .
| __STATIC_INLINE uint32_t MSC_IntGetEnabled | ( | void |
|
) |
Get enabled and pending MSC interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
- Note
- Interrupt flags are not cleared by the use of this function.
- Returns
-
Pending and enabled MSC interrupt sources The return value is the bitwise AND of
- the enabled interrupt sources in MSC_IEN and
- the pending interrupt flags MSC_IF
Definition at line
279
of file
em_msc.h
.
References MSC .
| __STATIC_INLINE void MSC_IntSet | ( | uint32_t |
flags
|
) |
Set one or more pending MSC interrupts from SW.
- Parameters
-
[in] flagsMSC interrupt sources to set to pending. Use a bitwise logic OR combination of valid interrupt flags for the MSC module (MSC_IF_nnn).
Definition at line
295
of file
em_msc.h
.
References MSC .
| MSC_RAMFUNC_DEFINITION_END MSC_RAMFUNC_DEFINITION_BEGIN MSC_Status_TypeDef MSC_MassErase | ( | void |
|
) |
Erase entire flash in one operation.
- Note
- This command will erase the entire contents of the device. Use with care, both a debug session and all contents of the flash will be lost. The lock bit, MLW will prevent this operation from executing and might prevent successful mass erase.
Definition at line
1127
of file
em_msc.c
.
References MSC , MSC_MASSLOCK_LOCKKEY_LOCK , MSC_MASSLOCK_LOCKKEY_UNLOCK , MSC_STATUS_BUSY , MSC_WRITECMD_ERASEMAIN0 , MSC_WRITECMD_ERASEMAIN1 , MSC_WRITECTRL_WREN , and mscReturnOk .
| __STATIC_INLINE void MSC_StartCacheMeasurement | ( | void |
|
) |
Starts measuring cache hit ratio.
This function starts the performance counters. It is defined inline to minimize the impact of this code on the measurement itself.
Definition at line
308
of file
em_msc.h
.
References MSC , MSC_CMD_STARTPC , MSC_IF_CHOF , and MSC_IF_CMOF .
| MSC_RAMFUNC_DEFINITION_END MSC_RAMFUNC_DEFINITION_BEGIN MSC_Status_TypeDef MSC_WriteWord | ( | uint32_t * |
address,
|
| void const * |
data,
|
||
| uint32_t |
numBytes
|
||
| ) |
Writes data to flash memory. This function is interrupt safe, but slower than MSC_WriteWordFast() , which writes to flash with interrupts disabled. Write data must be aligned to words and contain a number of bytes that is divisable by four.
- Note
- It is recommended to erase the flash page before performing a write.
It is recommended to run this code from RAM. On the Gecko family, it is required to run this function from RAM.
For IAR, Rowley, SimplicityStudio, Atollic and armgcc this will be achieved automatically by using attributes in the function proctype. For Keil uVision you must define a section called "ram_code" and place this manually in your project's scatter file.
This function requires a system core clock at 1MHz or higher.
- Parameters
-
[in] addressPointer to the flash word to write to. Must be aligned to words. [in] dataData to write to flash. [in] numBytesNumber of bytes to write from flash. NB: Must be divisable by four.
- Returns
-
Returns the status of the write operation
* flashReturnOk - Operation completed successfully. * flashReturnInvalidAddr - Operation tried to erase a non-flash area. * flashReturnLocked - Operation tried to erase a locked area of the flash. * flashReturnTimeOut - Operation timed out waiting for flash operation * to complete. Or the MSC timed out waiting for the software to write * the next word into the DWORD register. *
Definition at line
1061
of file
em_msc.c
.
Referenced by nvm3_halWriteWords() , and NVMHAL_Write() .
| MSC_RAMFUNC_DEFINITION_END MSC_RAMFUNC_DEFINITION_BEGIN MSC_Status_TypeDef MSC_WriteWordFast | ( | uint32_t * |
address,
|
| void const * |
data,
|
||
| uint32_t |
numBytes
|
||
| ) |
Writes data to flash memory. This function is faster than MSC_WriteWord() , but it disables interrupts. Write data must be aligned to words and contain a number of bytes that is divisable by four.
- Note
- It is recommended to erase the flash page before performing a write. It is required to run this function from RAM on parts that include a flash write buffer.
For IAR, Rowley, SimplicityStudio, Atollic and armgcc this will be achieved automatically by using attributes in the function proctype. For Keil uVision you must define a section called "ram_code" and place this manually in your project's scatter file.
- Parameters
-
[in] addressPointer to the flash word to write to. Must be aligned to words. [in] dataData to write to flash. [in] numBytesNumber of bytes to write from flash. NB: Must be divisable by four.
- Returns
-
Returns the status of the write operation
* flashReturnOk - Operation completed successfully. * flashReturnInvalidAddr - Operation tried to erase a non-flash area. * flashReturnLocked - Operation tried to erase a locked area of the flash. * flashReturnTimeOut - Operation timed out waiting for flash operation * to complete. Or the MSC timed out waiting for the software to write * the next word into the DWORD register. *
Definition at line
1104
of file
em_msc.c
.